In the course of more ecological and sustainable lifestock farming it is necessary to monitor the environmental and health conditions of the animals.
Acceleration sensors and LTE mobile radio modules including localization (GNSS) by Würth Elektronik can be used to implement monitoring applications. In case the sensor system detects the movement pattern of an animal, an alarm signal will automatically be sent or predefined persons could be contacted if an abnormal behavior is detected. humidity sensors can be used to monitor the status of the environment.
Wi-Fi modules can be integrated to connect the hook strap to the gateway Bluetooth LE to read out the measurements via smartphone. Data can be collected and finally send to the cloud using AWS or Azure.
Benefits
Bluetooth
Proteus-III
Connect from smartphone to the hook strap to transfer data from the cow.
Long-Range-Wan
Daphnis-I
Cost-effective connection of dozens or hundreds of sensors to one gateway.
Cellular & Positioning
Adrastea-I
Cloud connection for datas and alarm and localization of the cow.
Climate change, loss of arable land, ever scarcer resources and a growing world population. There are more and more challenges in food production. New approaches are being sought to meet these challenges. One of them is smart farming.
With our WE line of FeatherWings you can rapidly prototype your own smart farming application. With the help of the Sensor FeatherWing you can measure data points such as temperature and humidity to check if the plants are feeling most comfortable.
This created data can be sent into any cloud using the Calypso Wi-Fi FeatherWing. On GitHub, we are providing quickstarts and examplecode to get data into Microsoft and Amazon IoT platforms. Here, the data can be displayed, stored and analyzed to optimize plant output.
Benefits
Actuators can now be controlled manually or automatically via RPC.
Create Data
Sensor FeatherWing
Sensing environmental conditions like temperature and potting soil humidity
Send Data
Calypso WiFi FeatherWing
Sending the collected data from the
sensors into the cloud platform
Illumination
WL-SMDC
WE can create target light recipes that promote specific quality parameters of the plant, such as improved root development, increased biomass etc.
Power
WPME-LDHM
MagI3C Power Module - a fully integrated constant current LED driver with PWM and analog dimming.
Professional power tools have to perform at high levels and must be able to endure a tough workload. The Industrial Internet of Things enables better management of expensive tools via wireless communication. In conjunction with sensors that monitor appropriate use, new business areas, such as the leasing of equipment, are opening up.
The slim and energy-saving Wi-Fi and Bluetooth modules from Würth Elektronik make power tools capable of communicating. The devices can be linked up anywhere - in the workshop, in the vehicle, or on the construction site. In conjunction with temperature, humidity and motion sensors, the tools become smart. They can transfer data concerning usage and wear to a cloud application for instance. The advantage: maintenance cycles can optimally be scheduled, and rental equipment can be billed based on actual usage. Furthermore, inappropriate use or damage can additionally be detected with the help of sensors.
Benefits
Power tools capture data concerning the usage and share it wirelessly
Bluetooth
Proteus-III
Connection between the tools which want to be used in Sync Mode. In Sync Mode, one master tool controls the other(s). Meaning, activating this tool via the tool trigger will activate the synchronized tool(s) as well.
Humidity & Temperature
WSEN-HIDS
Sensing Humidity & temperature of the environment to ensure the vacuum cleaner is used in right operating conditions.
WIFI
Calypso
Connect the control unit to Internet: Cloud connectivity for status information, changes to the settings from anywhere in the world.
Cellular
Adrastea-I
Connect the control unit to Internet: Cloud connectivity for status informations, changes to the settings from anywhere in the world etc.
Combined
Stephano-I
Possibility to connect devices directly to the internet via WiFi and to smart devices via Bluetooth®.
The interconnection of power tools offers various advantages and applications. Especially with battery-powered tools there is no longer a connection between the tools, which does not allow a synchronized function.
With the help of Bluetooth networking, the various tools can be operated in coordination with each other. For example, a vacuum cleaner starts as soon as the drill is started. Ideally, the various functions can be controlled with the help of an app.
Via a mobile device, it is possible to download the usage and wear data, and as a result to optimally plan the maintenance cycles or, in the case of a rental device, to settle the accounts on the basis of actual usage.
Benefits
Humidity & Temperature
WSEN-HIDS
Sensing Humidity & temperature of the environment to ensure the vacuum cleaner is used in right operating conditions.
Bluetooth
Proteus-III
Connection between the tools, which want to be used in Sync mode: Sync mode one master tool controls the other(s). Meaning, activating this tool via the tool trigger will activate the synchronized tool(s) as well.
In the case of motorcycle accidents, it is of crucial importance to receive medical aid as soon as possible, as the collision might severely hurt internal organs. A smart helmet that can detect a crash and send an emergency alarm automatically could thus be a lifesaver.
Acceleration sensors and LTE mobile radio modules including localization (GNSS) by Würth Elektronik can be used to implement safety applications. In case the sensor system detects the movement pattern of a collision, an emergency call will automatically be sent or predefined persons could be contacted.
Benefits
A helmet which is able to communicate and to collect data can increase safety and comfort of the biker.
Humidity & Temperature
WSEN-HIDS
Measuring environmental conditions in the helmet to avoid overheat in summer time or wetness in the helmet due to leakage while siginficant rain.
Acceleration
WSEN-ITDS
• Impact detection and initiationg the radio module to setup an emergency call.
• Impact detection to gather information for the doctors for the grade of injury.
• Concussion detection
Bluetooth
Proteus-III
Connection from helmet to mobile to download. Data from helmet like head movement, specific vibrations, etc.
Cellular & Positioning
Adrastea-I
Communication of data inclusive
localization (GNSS) to predefined
receiver.
Automatic Guided Vehicles (AGV) or Autonomous Mobile Robots (AMR) are vitally important for flexible intralogistics concepts. While GNSS can be used for navigation outdoors, robots in factories and warehouses need different orientation techniques.
Key factors for the navigation of AMRs are wireless communication and acceleration sensors for inertial navigation. Würth Electronic does not only offer sensor and radio modules but also supports various communication protocols. Orientation via anchor point antennas distributed on the factory or warehouse floor as well as transmission of orders and status updates can be realized, e.g. with Bluetooth, Wirepas Massive Routing Mesh, or WE-ProWare Flooding Mesh.
Benefits
Autonomous Mobile Robots – autonomous but well connected
Proprietary
Tarvos-III
Sub-GHz radio communication in industrial environment offers reliability.
Bluetooth
Proteus-III
Find a specific robot selected using the function “Direction Finding” to navigate the user to the tool.
Mobile lighting at construction sites, especially on expressways, pose a great risk to the workers, if these lights are shifted by unobservant road users. Sensors and a communication mesh provide additional safety.
The lamps and warning beacons for road construction have sensors for detecting strong movement impulses (impact) as well as for location detection. The lamps are interconnected via a mesh network and report any change in location within a centimeter range. This eliminates the need for regular checks along the site to ensure that all luminaires are still in the right position. The interconnection of the luminaires can be realized with a Wirepas Massive Routing Mesh, or WE-ProWare Flooding Mesh by Würth Elektronik.
Benefits
Smart lamps form a mesh and control their own position
Humidity & Temperature
WSEN-HIDS
Sensing Humidity & Temperature to be aware of true local weather conditions.
Cellular & Positioning
Adrastea-I
Communication from Master Gateway at construction site to central server and getting location through GNSS Service.
Long-Range-Wan
Daphnis-I
Connection of dozens or hundrets of devices over long distance.
Mesh
Thetis-I
Connecting hundreds of devices to extend the range and without having the need to add LTE with recurring costs to each device
Proprietär
Thyone-I
Use a remote control connected wirelessly to the lamps and adjust settings.
Runway firing requires the highest reliable synchronized lighting. Reducing the wiring lowers installation costs and improves the degree of scalability.
Easy integration of new windmills into the existing park requires a reliable and secure bidirectional radio communication to increase Green Energy sector.
Würth Elektronik offers a variaty of GNSS Moduls not only for localization but also for time synchronization. In combination with globally accepted radio standards like Wi-Fi, Bluetooth, WE-ProWare, NB-Iot and LTE Cat. M the far distance management of machines, meaning remote monitoring and controlling, gives you dependend on the application either worldwide or locally enclosed access to your devices. In both cases highest security requirements can be fulfilled.
Predictive and curative maintenance can be triggered by intelligent digital sensors giving you the status of the environmental conditions in- and outside the housing and provides protection against natural destruction and exceptional failures.
Data can be made acessable through secure cloud connectivity.
Benefits
Adrastea-I
Far distance maintenance access – remote control. Time Synchronization between different lights. Time Stamping for Events.
Proprietary
Setebos-I
Proprietary for secure Mesh connection of the lighting network. Combined with Bluetooth for individual lighting configuration.
Humidity & Temperature
WSEN-HIDS
Environmental condition tracking within the lights. Recogninzing exceptional conditions like penetrating moisture.
Acceleration
WSEN-ITDS
Detection of shock and mechanical influence and stress, like bird pecking.
Coffee machines are popular and in daily use. Modern machines allow creative compositions of personalized coffee variants. At the same time, leasing models are increasingly based on so-called wet hours or actual consumption – smart solutions are required.
Humidity and temperature sensors as well as Bluetooth, WiFi and cellular modules from Würth Elektronik: Equipped in this way, a coffee machine can become a smart device. With the help of integrated humidity and temperature sensors, it is possible to control the machine’s optimal functioning. A change of the machine's values indicates a malfunction, which means that the need for maintenance can be displayed at an early stage or reported directly to a service center. In leasing, a billing system can be realized through live data transfer to the cloud. Convenient for the user: By using a mobile app, each user can design his or her personal coffee and preset, e.g. the amount of coffee, milk, or water.
Benefits
Coffee pleasure with pay per use
Humidity & Temperature
WSEN-HIDS
Measuring Humidity and Temperature ensures an optimal function and taste.
Bluetooth
Proteus-III
Connect to mobile App to preset your personal coffee or also as service interface for the technician.
Combined
Stephano-I
Connecting to the internet via WiFi and to end users smart devices via Bluetooth®.
Older houses often have many weak points and are particularly vulnerable to burglary. However, retrofitting wired security devices is expensive and laborious. Manufacturers should therefore also offer radio-based alarm systems.
The development of retrofittable alarm systems with wireless technology depends on the right combination of radio technologies. For the control system, a connection to the Internet or to the mobile network is required. For connecting the sensors, radio frequencies in the sub-GHz and the 2.4 GHz range can be used, whereas both short and longer distances have to be bridged. Due to security reasons, the use of a long-established but not publicly known radio protocol, such as WE-ProWare by Würth Elektronik, is very advantageous. Intelligent sensor technology can detect the opening of windows or doors by measuring the change in barometric pressure, temperature or humidity and trigger a silent alarm.
Benefits
Proprietary radio protocol – a security advantage
Proprietary
Tarvos-III
The flooding mesh network of the WE-ProWare offers hundreds of alarm sensors to be connected secure and reliable.
Proprietary
Thyone-I
The flooding mesh network of the WE-ProWare offers hundreds of alarm sensors to be connected secure and reliable.
Bluetooth
Proteus-III
Accessing the alarm system settings from a mobile device in a short range.
Cellular
Adrastea-I
Connecting the alarm system main console to the cellular network.
Combined
Setebos-I
Interconnecting all sensors through the WE-ProWare mesh, while offering mobile device access through Bluetooth in one device.
Humidity & Temperature
WSEN-HIDS
Measuring local room temperature & humidity simultaneously.
Acceleration
WSEN-ITDS
Recognizing movement of particular inventory like expenisve art.
Absolute Pressure
WSEN-PADS
Measuring local room air pressure to monitor unforeseen window openings e.g. during a burglary.
Electronic devices such as motion detectors or video cameras for surveillance purposes which are installed in public or easily accessible areas are particularly at risk. Criminals will always try to destroy these devices first. Therefore, the intentional destruction of such electronic devices must be detected and reported immediately.
To be able to detect any tampering with a surveillance device, a sensitive 3D acceleration sensor and a radio module should be integrated. With the highquality and power-saving components from Würth Elektronik, solutions can be developed that immediately sound the alarm, if someone tampers with a surveillance camera or motion detector.
Benefits
Protect the protecting devices
Acceleration
WSEN-ITDS
Sensing Acceleration for vandalism protection. Tamper detection is the ability of a device to sense an active attack to the device and the threat of the attack should initiate an event (e.g. alarm, shutdown of the device).
Power
WPME-VDMM
MagI3C power module - a fully integrated DC-DC converter. High power density for a Cool design. Adjustable output.
Illumination
WI-SIQW
IR LEDs are uses to illuminate areas with infrared light, which is invisible to the human eye but can be detected by special cameras.
Smart homes need smart washing machines. Only a washing machine which is connected to the Internet of Things can be controlled remotely and switched on, for example, when there is a surplus of energy from the house's solar panels. Really smart machines come with excellent sensors.
Manufacturers who make their washing machines "intelligent" are opening up completely new business models. Machines that receive commands and provide feedback wirelessly can be sold as components of smart home concepts. If absolute pressure, differential pressure, temperature, and acceleration sensors are used to monitor the correct operation of a washing machine, leasing models can be developed, in which the customer only pays for actual use, for example in a laundromat or communal laundry. At the same time, the machine automatically reports the need for maintenance, for example, when its vibration behavior changes the material.
Benefits
Laundry becomes more sustainable
Absolute Pressure
WSEN-PADS
Measuring the water level through pressure in the washing cabine.
Humidity & Temperature
WSEN-HIDS
Measuring humidity & temperature in the drum while drying process.
Differential Pressure
WSEN-PDUS
Measuring the pre- and post-pressure of a filter to detect filter contamination.
Acceleration
WSEN-ITDS
Monitoring and analyzing a possible unbalance of the washing drum.
Bluetooth
Proteus-III
Bluetooth connectIvity for mobile control or as technician interface.
Combined
Stephano-I
Connecting to the internet via WiFi and to end users smart devices via Bluetooth®.
LCDs are often used to indicate the status of devices, machines, and factory equipment. A little LCD Monitor on a machine looks elegant but it is not necessarily a sensible solution. LCDs age faster under harsh conditions and are wasteful in applications where they only need to be read a few times a year. Better: wireless data retrieval.
Anyone who provides machines or industrial plants with Liquid Crystal Displays should always consider whether such a display is necessary at this point, especially because every person who comes to the machine today carries a device with much higher display quality. With the industrial grade Bluetooth, WiFi and cellular modules from Würth Elektronik, it is easy to replace LC displays and output information to a mobile device app instead.
Benefits
Use your phone to check the machine
Bluetooth
Proteus-III
Make use of the screen from a mobile device while saving the cost of an integrated LC display in the machine.
WIFI
Calypso
Using the WiFi direct function to use a responsive website instead of Bluetooth.
Combined
Stephano-I
Possibility to connect via WiFi to the internet and via Bluetooth® to end users smart devices.
Cellular
Adrastea-I
Connect an off-site machine to the internet through a cellular network. Save the LC display cost and lower the amount of possible damageable components.
Send Data
Calypso WiFi FeatherWing
Sending the collected data from the sensors into the cloud platform
Create Data
Serial Bridge FeatherWing
Sensing environmental conditions like temperature and potting soil humidity
Rotary switches on control units were a sensible solution for a long time. Furthermore, there was always the risk of unauthorized use. The more modern and secure approach: make the control unit addressable via radio. Or even make it an IoT device.
The ubiquity of smartphones and the widespread use of Wi-Fi networks open up the possibility of dispensing with rarely used switches on control units. With the slim Bluetooth LE and Wi-Fi modules from Würth Elektronik, you can make your control unit capable of wireless communication. The big advantage: Access can be restricted by secure authentication. And where a connection already exists, it can also be used to update the control unit, or for management via the Internet.
Benefits
Use your phone to activate the switch
Bluetooth
Proteus-III
Replace the rotary switches with BT-LE and connect to Mobile device. Avoid external changes to the control unit. Advantages like Authentification needed for changes. Mobile device can update control unit main functions.
WIFI
Calypso
Connect the control unit to Internet. Cloud connectivity for status informations, changes to the settings from anywhere in the world etc.
Create Data
Serial Bridge FeatherWing
Sensing environmental conditions like temperature and potting soil humidity.
Send Data
Calypso WiFi FeatherWing
Sending the collected data from the sensors into the cloud platform
Building automation is a great way to make indoor living more comfortable while saving energy. Lighting, heating, and ventilation systems only become really smart when they are adequately interconnected.
Sensors for humidity, temperature or CO² are needed to measure indoor air quality, as are connections to heating and ventilation systems, automatic window opening and shading systems. WiFi is suitable for connecting the gateway to the Internet for remote control, while mesh networks such as WE-ProWare are state of the art for interconnecting all sensors and actuators, light switches, and air conditioners.
Benefits
Mesh networks to control the ambience
Combined
Setebos-I
Interconnecting all sensors through the WEProWare mesh, while offering mobile device access through Bluetooth in one device.
Humidity & Temperature
WSEN-HIDS
Measuring local room temperature & humidity simultaneously.
Acceleration
WSEN-ITDS
Recognizing movement of particular inventory like expenisve art.
Absolute Pressure
WSEN-PADS
Measuring local room air pressure to monitor unforeseen window openings e.g. during a burglary.
A green garden is the jewel of any private or public building. But irrigation should be managed wisely. Especially in times of water scarcity, only as much water as necessary should be fed into the sprinkler system. With connectivity and sensors, sprinkler systems become intelligent.
A smart water pump detects when it is the right time to water the garden – based on wirelessly connected soil moisture sensors, the time of day, and maybe even from data about the availability of water resources like a cistern. By using several intelligent water pumps, gardens or parks can also be partially irrigated. Developers of irrigation systems should consider using humidity sensors and connectivity solutions like WE-ProWare Flooding Mesh or Wirepas Massive Routing Mesh to offer smart solutions which help their customers to save water.
Benefits
Mesh networks to control sprinklers
Humidity & Temperature
WSEN-HIDS
Sensing outdoor humidity and temperature directly at the required planting bed.
Acceleration
WSEN-ITDS
Sensing Accelaration for vandalism protection. Theft protection in case of movement.
Mesh
Thetis-I
Connection of hundreds of intelligent water sprinklers through a battery-saving routing mesh.
Long-Range-Wan
Daphnis-I
Connecting devices over big distance and sending data to a gateway.
Who does not know it - forgot the key and locked out. Furthermore, they are uncomfortable in the pants or get lost in the handbag.
With the help of a unique assignment via Bluetooth and the appropriate app, such door opening systems are both secure and comfortable using a mobile device.
Benefits
Acceleration
WSEN-ITDS
Sensing Acceleration for vandalism protection, e.g. tamper detection
Power
WPME-VDMM
MagI3C power module - a fully integrated DC-DC converter. High power density for a Cool design. Adjustable output.
Signal Indicator
WL-ICLED
ICLEDs allow for precise colour and brightness customization. They enable dynamic lighting effects and colour sequences with just a single data line.
Connection
WR-MJ
Connect the Smart Power Distribution and Relay Controller to the home internet gateway.
Equipping public buildings such as schools with air filtration devices to prevent infection, has burdened facility managers with an additional maintenance task. Manufacturers of such equipment would do well to simplify maintenance and operation – only a properly working air filter will protect.
The more air filters are in use, the more important remote maintenance becomes. Differential pressure and humidity sensors can be used to monitor the status of the filters. An internet gateway and a cloud application make remote maintenance convenient. Wi-Fi modules can be integrated to connect the devices to the gateway. A particularly flexible solution is an 868 MHz radio module with the proprietary radio protocol WE-ProWare. Additionally, this allows the bridging of longer distances than with Wi-Fi, if necessary.
Benefits
Proprietary network for remote maintenance
WIFI
Calypso
Using the WiFi direct function to use a responsive website instead of Bluetooth or simply connect the filter directly to the internet.
Proprietary
Tarvos-III
Connecting several Air filter in large building with each other through a mesh network. Sub GHz because of LongRange and sending data through walls.
Acceleration
WSEN-ITDS
Sensing Acceleration for vandalism protection, e.g. tamper detection.
Differential Pressure
WSEN-PDUS
Measuring the pre- and post-pressure of a filter to detect filter contamination.
Agriculture, biogas plants, haulers and industrial enterprises - there are many areas of application for a mobile axle load scale. When driving over it, the load on each single wheel of the vehicle is weighed separately. The measured values must then be merged.
In the case of mobile axle load scales, the weighing program calculates the total weight via the weighed axles. For this purpose, the individual scales must be linked by radio. Using a mesh network between the scales, the data can be collected and sent to a mobile device. Software in an mobile App can calculate the center of gravity of the load. Connecting the networked scales to the Internet and equipping them with GPS modules makes the management of the stock of these devices as simple as possible.
Benefits
Mesh-network of wheel scales
Combined
Stephano-I
WiFi and Bluetooth® connectivity for internet connection and controlling application via Bluetooth®.
Combined
Setebos-I
Mobile App Connectivit Sending weight data through mobile App. Mesh between 4 scales for each wheel.
Acceleration
WSEN-ITDS
Sensing Acceleration for vandalism protection or to avoid theft.
Even during the pandamic, there were more than 150 Million containers shipped during 2021. It has never been as important to know, where your containers are, as it is at the moment! Due to shortages of materials, the bottle necks on asian harbors and during an pandemic, it is crucial to be aware of what happens with your products and where they are.
With the Wirepas Mesh Network communication protocol every device can be used as wireless router and can act as a repeater for other nodes. With WE sensors it's possible to monitor the environmental conditions of your parts just in time, any time. The GNSS modules allow to follow the tracked container and give you an excat location of your parts. A network out of thousands of nodes, i.e. containers, increases the scale of the whole network and following the distance to bridge. Wirepas Massive offers a so called Positioning engine which is helpful to locate containers even inhouse.
Benefits
Humidity & Temperature
WSEN-HIDS
Measuring container internal or outdoor temperature & humidity simultaneously.
Cellular & Positioning
Adrastea-I
Connecting the container tracking to the cellular network and the location can be tracked wherever the container is on the globe.
Acceleration
WSEN-ITDS
Sensing Acceleration and impacts to have the information available when a container starts moving or in case a huge damage to the load has occured.
In this country local laws govern and limit usage of pesticide. In order to comply with environmental laws, a black box on the tractor monitors the amount of pesticide dispensed on the land allocated to the farmer. This way the amount of sprayed pesticide is controlled and overdosing is avoided.
In the pump box of the sparying installation mounted on the tractor, a radio module receives data from the spray nozzles. Every nozzle is fitted with differential pressure sensors monitoring an equal flow, and their radio module transmits in the correct time slot the flow figure. In the central unit the metrics are computed in order to match the volume of pesticide to the surface on which the tractor has covered.
To refine the calculation, GNSS can be added to match the volume to the land surface, and NB-IoT / LTE-M can be implemented in case the governing authority requests that the data should be stored on a server.
Benefits
Quick win of using a radio module or a sensor
Differential Pressure
WSEN-PDUS
Measuring & Monitoring an equal dispensing across different nozzles.
Cellular & Positioning
Adrastea-I
Enabling direct cloud access through cellular technology makes predicitive maintenance real.
Proprietary
Telesto-III
Collecting and sending data from sensor nodes in the pesticide spray system and transmitting those values to the cellular gateway For US customers, the 868 MHz radio module can be replaced by its 915 MHz pin- and software compatible counterpart, Telesto-II.
Acceleration
WSEN-ITDS
Predictive Maintenance means checking the system if there are any notices of spraying arms unbalance.
Road side safety barriers ensure safety of pedestrians
and traffic during construction and in case of accicdents.
Often these cones get displaced posing a threat to human
life. Retrofitting these barriers with sensors ensures early
detection of displacement thereby saving human lives.
An acceleration sensor can be used to detect a fall of a safety barrier and
a positioning system accurately determines the position and timing of the
barrier. This data can be transmitted via cellular link to a data platform. A
cloud platform can be further used to analyse and notify the operator to
take corrective action when necessary.
Benefits
Cellular & Positioning
Adrastea-I
Connect the control unit to the internet: Cloud connectivity for status informations, changes to the settings from anywhere in the world etc. and localization of each single unit in case of theft or finding all owned units.
Combined
Setebos-I
Interconnecting all sensors through the WE-ProWare mesh, while offering mobile device access through Bluetooth in one device.
In a sustainable world where e-mobility becomes more and more important and dominant, added services through connectivty solutions are crucial to differentiate from others. Easy usage of an e-bike for any user – if it is your personal or
a rental bike – can be simply ensured using technologies like LTE, Bluetooth & GNSS.
Instead of an attached fixed display, the control is simply done via smartphone.
A Bluetooth Connect app is the smart Control Center and so the smartphone
clearly displays the navigation and bike status and control even in daylight.
Electronic locking can be performed and the cyclist can access diagnostics
and support information for the bike. Once the settings are made, the engine
automatically remembers the last rides settings.
It allows you to safely and freely explore the new road.
Thanks to a constant LTE connection, GPS tracking allows constant monitoring
of the e-bike's position. Even in the worst case of theft, users around the world
can be helped to get their beloved e-bike back
Benefits
Cellular & Positioning
Adrastea-I
Access to all data (service and status Information) from anywhere in the world added by Live Tracking Signal of the e-bike / vehicle across the globe.
Combined
Setebos-I
Bluetooth function of the combined module to connect all control units on the bike like shifter etc. Secure proprietary mode for service personal only, to upload specific FW updates to e.g. the motor.
Humidity & Temperature
WSEN-HIDS
Environmental condition tracking within the battery or the engine. Recogninzing exceptional conditions like penetrating moisture.
Acceleration
WSEN-ITDS
Detection of shock and mechanical influence and stress. Recognizing movement of the e-bike while being suposed to be stationary.
Gyro
WSEN-ISDS
Measuring the orientation of the bike. Can be used as compass to enhance the navigation.
As e-mobility will be more and more a key for sustainable transportation, future charging infrastructure has to be both, smart and easy to use and also future proof and connected.
specially the connection between different charging stations with each other and also the charged devices have to be able to communicate with the infrastructure directly. Additionally there is a third party in here – the human wishing to be able to communicate with the infrastructure and expressing his plans and wishes. All that can be achieved with clever communication possibilities: Connecting the charging stations with each other could be reached with clever mesh solutions, so that there is no additional wiring needed. Communicating with the cars themselves could be done via cellular communication. The direct communication to the user could be implemented either also via celluar or with direct Bluetooth or WiFi Interface. With smart MEMS sensors, a bunch of information could be generated to know as much as possible of the device. For Payment cases there could also be the need of widespread communication standards as wM-Bus gives the possibilty to communicate standardized to Smart Meter Gateway (SMGW).
Benefits
Acceleration
WSEN-ITDS
3D-orientation and TAP detection as input method for the screen.
Humidity &Temperature
WSEN-HIDS
Environmental condition like penetrating moisture or over temperature leading to a reduced charging power.
Residual Current
WE-RCDS
Residual current detection sensor designed for wallboxapplication to meet IEC 62955: 2018.
Cellular & Positioning
Adrastea-I
Far distance maintenance access – remote control and exact location of the charging station as well as exact timing information for synchronisation.
Wireless M-Bus
Metis-II
Wireless connection to read out multiple meters without wiring effort.
Wirepas
Thetis-I
Meshing up multiple charger stations for balancing the load effectively.
WIFI / Bluetooth
Stephano-I
Connectivity as service interface and for taking into operation.
With the newest sport equipment you can track your training status, choose your favorite mode and connect yourself with other users. Connecting punching balls, dumbbells, balls and lot more allows a smart way to connect the personal training to friends and colleagues and brings a high motivation in competeting each other.
Würth Elektronik offers Bluetooth and WiFi to connect the smartphone to your favorite sport device. Quantities of pushes, measuring strength of a hit or counting time of a movement is all digital information, you did not have in the past in personal training. With this data it is possible to empower the athlete in documenting and recognising changes and developments as well as there is the possibility of competeting. MEMS acceleration sensors are a very easy and cost effective way to raise this information. With Bluetooth Low Energy this data can be sent easily to the users smart device and directly into a competition cloud. Highest security requirements can be fulfilled.
Benefits
Bluetooth
Proteus-e
Transfer data to the smartphone like:
With raising technologie possibilities also the housekeeping gets more and more automated, intelligent and more comfortable. To do so, a lot of sensors and connectivity functions are needed. All data has to be sent via WiFi through the internet to userfriendly server applications.
In smart cleaning devices a lot of physical values are of interest. Temperatures have to be monitored, pressures, esp. for vacuums, have to be checked. You have to be sure, no humidity attacking your device. And lot more.
With Würth Elektronik digital MEMS Sensors there is a bunch of possibilities to collect data. Data of course is only useful if you know how to use it. Therefore a communication to the device itself but also to the controlling user or cloud systems above is important. With Bluetooth a communication directly to a smart device is easy and a taking into operation is possible without problems. WiFi enables to sent the data into a cloud and then to send back again to the user. And also brand new technologies like Matter can be integrated with radio modules.
Benefits
Acceleration
WSEN-ITDS
Easy detection of static or moving devices for energy saving and reactivation.
Bluetooth
Proteus-e
Transfer data to the smartphone like:
Differential Pressure
WSEN-PDUS
Sensing the pneumaticm pressure inside vacuumm cleaner applications.
Batteries are driving our world. Especially in the consumer field. Remotes, toys and lots of other devices only work with energy out of batteries. Technologie enables a lot possibilities in monitoring devices and also their batteries to be able to charge or exchange them in time. Ageing batteries behave differently and carry the risk of leackage or function loss.
Sensing temperature and in some cases also humidity is the first step to get information about the used battery above the only voltage level. If you also check movement of a device with the acceleration sensors and with this offer the possibility to easily detect whether the device is moving or not. With this information, the intelligent battery can shut down devices not in use and both save energy. The integrated functionality of the sensor can wake up a microcontroller behind only as the device is moving. Beyond that, not only the device itself can be interested in the information, also the user could use the information about the battery condition and therefore connect via Bluetooth or WiFi to the device or directly to the battery to detect the needs of the application.
Benefits
Temperature
WSEN-TIDS
Precise measuring the temperature in battery cells to avoid overheating and ensuring devices operating inside them specified conditions.
Humidity & Temperature
WSEN-HIDS
Environmental condition tracking within the device. Recogninzing exceptional conditions like penetrating moisture.
Acceleration
WSEN-ITDS
Detection of movement and possible damage because of crash with freefall detection.
Bluetooth
Proteus-e
Transfer data to the smartphone like:
With more and more renewable energies in the public power grid also the need of information about the produced energy, as well as the needed power, has to be increased significantly. Only with data the energy transformation could be managed.
With energy meters it is possible to detect energy consumptions as it is done for years. But as there are more and more decentralized energy providers producing green energy, more information is needed to transport the energy and also to use the grid securely. The measured power flows, that‘s where it all begins. This information has to be collected efficiently, as the enery meters should not have a high energy consumption for themselves. The very different use cases also need very different solutions.
In areas, where a lot of energy meters are installed, you should collect data from all of them and bring it into a superordinate system at one point. Predictive and curative maintenance can be triggered by intelligent digital sensors giving you the status of the environmental conditions in- and outside the housing and provides protection against natural destruction and exceptional failures.
Data can be made acessable through secure cloud connectivity.
Benefits
Wireless M-Bus
Metis-II
Wireless connection to read out multiple meters without wiring effort.
Humidity & Temperature
WSEN-HIDS
Environmental condition tracking within the meters. Recogninzing exceptional conditions like penetrating moisture.
Bluetooth
Proteus-e
Connect from smartphone to the meter for taking into operation and as service interface.
The effectiveness of a solar panel is largely determined by the angle of incidence of the sun. If this angle can be dynamically adjusted, significantly higher energy yields are possible. Smart balcony power plants with batteries and wireless connectivity gives the customer insight and power to control his power usage and optimize it in order to make the most of his produced energy.
Adapting the angle of solar panels dynamically to the sun cann enlarge the profit out of the panel tremendously. Using MEMS Inerital Meauring Units (IMUs) gives the possibility of sensing the orientation of the panel in relation to the earth gravity and therefor allows to bring the panel in the perfect angle to the sun at every moment during the day. With this, the outcome can be increased easily.
By connecting multiple panels or groups of panels, the adjustment can be done simultaniously or intentionally not the same way. Using Bluetooth LE brings the opportunity to get a quick and easy access to the typical waterproof manufactured housings without effort for service or taking into operation.
LTE Cat.M conectivity allows alarming in case of malfunstions or damages caused by weather or animals (as i.e. sheeps are often used as lawn trimmers in these areas. Humidity sensor based on MEMS technology allews easy calyulation of dew point and whether there has to be activated any heaters in some kind of application.
Benefits
Gyro
WSEN-ISDS
Detection of movement, adjustion, shock and mechanical influence and stress, like bird pecking.
Humidity & Temperature
WSEN-HIDS
Environmental condition tracking like penetrating moisture.
WIFI / Bluetooth
Stephano-I
Connect from smartphone or a WiFi network to the panel for taking into operation and as service intereface.
In solar farms a permanently maintenance is required. This means to check the condition of the solar panels and inverters or to do some updates.
Würth Elektronik offers with the NB-Iot and LTE Cat. M connectivity the far distance management of the inverters, meaning remote monitoring and controlling, gives you either worldwide or locally enclosed access to your devices. In both cases highest security requirements can be fulfilled. If there is an firmware update for the inverter needed, this could be transfered via cellular too or via an service staff with Bluetooth in front of the inverter.
Benefits
Bluetooth
Proteus-III
Connect from smartphone to the inverter to transfer data from and to the inverter.
Long-Range-Wan
Daphnis-I
Connecting dozens or hundrets of systems to one gateway wirelessly.
Residual Current
WE-RCDS
Fault DC current detection in the system for fail-safe operation.
Humidity & Temperature
WSEN-HIDS
Environmental condition tracking within the inverters. Recogninzing exceptional conditions like penetrating moisture.
Acceleration
WSEN-ITDS
Detection of shock and mechanical influence and stress, like bird pecking.
It would be important in the power sector to be able to provide clean technology and embedded software solutions to reduce power consumption and costs, as well as retrofit monitoring for power line infrastructure and solar and weather station kits. The solutions then monitor power line fluctuations and deflections, as well as fire risk areas as fire detectors, and provide monitoring and smart city solutions for government agencies.
There is an exciting and rapidly changing atmosphere in the energy and utilities industry. The rapid adoption of new technologies, particularly communications-based technologies, is enabling them to better monitor, control and optimize every aspect of their business. There is no doubt that connectivity is the key to the smart grid. Wireless connectivity is enabling tomorrow's power plants and smart grids.
Wireless connectivity and network intelligence provide the ability to centrally monitor, self-regulate and respond to demand. Remote cameras and sensors reduce the need for on-site maintenance staff. Sensors enable near real-time diagnosis of expected and unexpected faults, enabling more accurate and faster fault location. Wireless connectivity provides reliable, accurate, and secure data from the field and offers cost and deployment advantages over competing technologies.
Benefits
Cellular & Positioning
Adrastea-I
Access to all monitoring and control data from anywhere in the world. Performing load balancing in the grid.
Wireless M-Bus
Metis-II
Sub-GHz radio communication with the wM-BUS EN13757 offers interoperability and reliability.
Long-Range-Wan
Daphnis-I
Long-range devices enable to install immediate prevention and control solutions in an established network.
Humidity & Temperature
WSEN-HIDS
Precise measuring the humidity & temperature at a specific point to avoid overheating and operating devices outside of the operational conditions.
Absolute Pressure
WSEN-PADS
Barometric pressure is one of the environmalental data which can forecast wheather conditions.
Temperature
WSEN-TIDS
Precise measuring the temperature at a specific point to avoid overheating and operating devices outside of the operational conditions
A CPAP machine is a machine that uses mild air pressure to keep breathing airways open while you sleep. The documentation process is very easy, if a wireless connection is established. Many people rely on such a machine and need medical support when evaluating the data. The current option of remote data transfer is a blessing, especially in rural areas with a low density of doctors.
With the well known radio standards like WiFi, NB-Iot and LTE Cat. M data can be simply transferred into a cloud system. Might this be a private solution or even a Cloud of a medical association with the highest security standards. Using the short range transfer capability of Bluetooth offers the patient the opportunity to evaluate the last night sleep on its own mobile device immediately in the morning.
For a digital spirometer in a handheld device size it is now possible to train the lung very well controlled at home. Expanding your lungs, strengthening your lungs, keeping your lungs inflated and clearing mucus and other secretions from your chest and lungs… all processes are precisely performed due to an App on your mobile device and a direct connection via Bluetooh. A well documented training progress is an added value as well.
Benefits
Differential Pressure
WSEN-PDUS
Measurement and monitoring of inhaled and exhaled air.
Humidity & Temperature
WSEN-HIDS
Precise control of the humidity in the inhaled and exhaled air, but also of the environment to process the right amount of humidity.
Cellular & Positioning
Adrastea-I
Transferring the measured data form any place in the world. Giving medial staff access to the machine to control or even adjust settings.
Bluetooth
Proteus-III
Connect from mobile device like smartphone to the CPAP machine or mobile spirometer for mobile app access, control function and firmware updates.
Bluetooth
Proteus-e
Connect from mobile device like smartphone to the CPAP machine or mobile spirometer form mobile app access.
WIFI
Calypso
Integrate the CPAP machine into a local WiFi network for cloud connectivity and immediate data transfer and analytics like alarms
In medical environments a lot of processes have to be followed and documentated correctly. Not rarely this means, that a well educated person has to do or document things, consuming a lot of time missing for the really important works to be done, mainly the time to care.
Würth Elektronik offers a variaty of globally accepted radio standards like WiFi, Bluetooth, WE-ProWare, NB-Iot and LTE Cat. M the far distance management of devices, meaning remote monitoring and controlling, gives you dependend on the application either worldwide or locally enclosed access to your devices. In both cases highest security requirements can be fulfilled.
Predictive and curative maintenance can be triggered by intelligent digital sensors giving you the status of the environmental conditions in- and outside the housing and provides protection against natural destruction and exceptional failures. Data can be made acessable through secure cloud connectivity.
Benefits
Gyro
WSEN-ISDS
Detection of any movement, orientation and acceleration of the device.
Humidity & Temperature
WSEN-HIDS
Environmental condition tracking within the lights. Recogninzing exceptional conditions like penetrating moisture.
Cellular & Positioning
Adrastea-I
Far distance maintenance access – remote control and documentation obligation.
New and better materials make it possible to produce increasingly robust, lighter and more durable prostheses and implants. The manufacturing und processing of these materials makes new processing methods necessary again and again
All moving machines like mills, lathes and CNC need an exact position and movement feedback. This could be realized with 6-Axis MEMS-Sensors from Würth Elektronik.
Pneumatic controlls need to be measured with high accuracy, i.e. with differential Pressure Sensors based on MEMS principles. These sensors are very accurate, temperature compensated and factory calibrated.
To get access to working machines without stopping automised processes, the service technican could connect wirelessly via Bluetooth or WiFi to the machine to read out running hours or fill levels or for calibrating the machine.
Benefits
Gyro
WSEN-ISDS
Detection of any movement, orientation and acceleration of the device.