On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik introduces its common-mode chokes for signal and data lines
Würth Elektronik is introducing another series of common-mode chokes for signal and data lines – WE-SLSP – combining high current and voltage ratings with a compact design. These SMT components feature a low package height of just 2.5 mm, a high rated voltage of 100 V, and low leakage inductance.
The new common-mode chokes are designed for applications with coupled data and power supply lines that require high signal integrity and electromagnetic compatibility where PCB space is limited. The component is available in versions with various rated currents and a wide range of impedance values at 100 MHz.
Variants for different impedance values
Applications for this particularly compact common-mode choke range from USB-C ports in consumer electronics, through PLC connections to 24 V to 48 V bus systems in industrial environments, to microinverters for renewable energy applications and 48 V PoE in telecommunications. The 5050 SMT package has a height of just 2.5 mm and its four terminals make it ideal for low-profile assemblies. WE-SLSP covers impedance values from 100 Ω to 2000 Ω at 100 MHz. The rated currents extend from 1.3 A to 6 A and, depending on the variant, the DC resistance is between 15 mΩ and 73 mΩ.
Free samples available now
All common-mode choke versions are now available from stock. As always, Würth Elektronik requires no minimum order value. Developers are welcome to request free samples.
Do you have any questions, comments or requests regarding our press work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here you can download the press information and pictures of the company area










Reference guides, technical reports and other information material
Würth Elektronik blog
Learn more about electrical design, new technologies and current innovations in our blog.