Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

30. July 2025
Components

Power Modules for Higher Current

Content you may also like

The MagI³C-VDLM power module family has been expanded with two LGA-26 SMDs offering output currents of 4 A and 5 A, respectively.

Würth Elektronik expands its MagI³C series with variable step-down modules featuring high current outputs

Würth Elektronik has expanded its successful MagI³C-VDLM power module series with two new models. With output currents of 4 A and 5 A respectively, they further enhance the performance of the existing portfolio of compact DC/DC power supply modules.

The new modules are designed for input voltages from 4 to 36 V and come in a space-saving LGA-26 package (11 × 6 × 3 mm). They provide an output voltage from 1 to 6 V and, like all power modules in the MagI3C-VDLM series, integrate the essential components for a DC/DC power supply in a compact package: switching regulator with integrated MOSFETs, controller, compensation circuitry, and a shielded inductor.

The power modules maintain high efficiency across the entire output current range by automatically switching between operating modes based on load requirements. So they ensure minimal output ripple – ideal for precise and interference-sensitive applications. Typical applications include point-of-load DC/DC converters, industrial, medical, test and measurement equipment, or for supplying power to DSPs, FPGAs, MCUs, MPUs, and interfaces.

Excellent efficiency

The MagI3C-VDLM modules achieve peak efficiencies of up to 96 percent and impress with their excellent EMC performance in accordance with EN55032 Class B / CISPR-32. Additional features include selectable switching frequencies, automatic PFM/PWM transition, and a sync function for synchronizing to individual clock frequencies.

The new MagI³C-VDLM modules are now available from stock without a minimum order quantity. All customers are offered design and layout reviews as well as EMI filter design support as a service.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company information for download

Here you can download the press information and pictures of the company area




Picture material for download

Publications

Reference guides, technical reports and other information material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik blog

Würth Elektronik blog

Learn more about electrical design, new technologies and current innovations in our blog.

You might also be interested in