Aluminum Hybrid Polymer Capacitors

Filter by values
 in 4 product lines for
Reset all
Filter
Filter by
 show  articles in 4 product lines
 articles in 4 product lines
Reset all
4 Product categories
WCAP-HTG5 General Purpose 105°C
WCAP-HTG5 General Purpose 105°C
C 10 to 470 µFVR 16 to 100 V (DC)
WCAP-HTAH Advanced High Temperature 125°C
WCAP-HTAH Advanced High Temperature 125°C
C 10 to 560 µFVR 16 to 100 V (DC)
WCAP-HSG5 General Purpose 105°C
WCAP-HSG5 General Purpose 105°C
C 10 to 560 µFVR 16 to 100 V (DC)
WCAP-HSAH Advanced High Temperature 125°C
WCAP-HSAH Advanced High Temperature 125°C
C 10 to 820 µFVR 16 to 100 V (DC)

Würth Elektronik capacitors

Big portfolio available ex stock

Würth Elektronik capacitors

Big portfolio available ex stock

Würth Elektronik has extended its capacitor portfolio. You will find an overview of our current technologies available ex stock in the graph. More details (e.g. series, characteristics, features, applications, etc.) about each product family can be found in the flyer or for example below. In our flyer you will also find information about our services.

Relationship between voltage and capacitance in the diagram

Aluminum hybrid polymer capacitors

Aluminum hybrid polymer capacitors

The Aluminum Hybrid Polymer Capacitors product family combines the technologies from our Aluminum Electrolytic and our Aluminum Polymer Capacitors. This results in the following features:

  • Low ESR
  • High ripple current characteristics
  • High stability over the temperature range
  • Low leakage current
  • High lifetime performance
alttext yt_img_for_code_QWAtpJq8qk4.jpg 1745391168

Available series

  • Series WCAP-HTG5

    • Mounting Style: Radial THT
    • Type: General Purpose 105 °C
    • Capacitance: 10 – 470 µF
    • Voltage:  16 - 100 V (DC)
  • Series WCAP-HTAH

    • Mounting Style: Radial THT
    • Type: High Temperature 125 °C
    • Capacitance: 10 – 560 µF
    • Voltage: 16 - 100 V (DC)
  • Series WCAP-HSG5

    • Mounting Style: V-Chip SMT
    • Type: General Purpose 105 °C
    • Capacitance: 10 – 560 µF
    • Voltage:  16 - 100 V (DC)
  • Series WCAP-HSAH

    • Montagetyp: V-Chip SMT
    • Typ: High Temperature 125 °C
    • Kapazität: 10 – 820 µF
    • Spannung:  16 - 100 V (DC)

Comparison of aluminum capacitors

Aluminium-Elektrolytkondensatoren

Aluminum electrolytic capacitors

  • Stable capacitance values at high temperature
  • High voltage ratings
  • Low leakage current
Aluminium-Hybrid-Polymer-Kondensatoren

Aluminum hybrid polymer capacitors

  • Low ESR
  • High ripple current characteristics
  • High stability over the temperature range
  • Low leakage current
  • High lifetime performance
Aluminium-Polymer-Kondensatoren

Aluminum polymer capacitors

  • Low ESR
  • High ripple current characteristics
  • High lifetime performance

Construction

Diagram showing the structure of three capacitors: Aluminum Electrolytic, Aluminum Hybrid Polymer, and Aluminum Polymer, each with anode, cathode, separator, and electrolyte.

Aluminum Capacitors

Aluminum Hybrid Polymer capacitors combines the technical advantages of aluminum electrolytic (e.g.: low leakage current) and polymer capacitors (e.g.: low ESR, high ripple current). These advantages can be realized through the mixture of the liquid electrolyte and the solid polymer.

An image showing the internal structure of the V-Chip SMT type, used in the WCAP-HSG5 and WCAP-HSAH series. Suitable for the reflow soldering process.

Inner Construction: V-Chip SMT

This internal structure of the V-Chip SMT type is used for our WCAP-HSG5 and WCAP-HSAH series. The V-Chip SMT mounting types are suitable for the reflow soldering process.

An image showing the internal structure of the WCAP-HTG5 and WCAP-HTAH series. The radial THT mounting types are suitable for wave soldering.

Inner Construction: Radial THT

The internal structure of our WCAP-HTG5 and WCAP-HTAH series is shown above. The Radial THT mounting types are suitable for wave soldering.

Example applications

Measurements

Redexpert

Measurements

Redexpert

With the help of REDEXPERT you will find the right capacitor based on your technical requirements. The tool supports, for example, with measured values for capacitance, impedance, ESR and dissipation factor (DF). The ability to compare individual components with each other in terms of measured values enables convenient component selection.

Computer screen with overlapping windows, graphs, and red 3D text: 'ONLINE PLATFORM BASED ON MEASURED VALUES.'
Graph showing the capacitance change as a function of temperature for three different types of capacitors: WCAP-HSGS, WCAP-PSHP, and WCAP-ASSH.
Graph showing the change of ESR (Equivalent Series Resistance) as a function of temperature for three different types of capacitors: WCAP-HSG5, WCAP-PSHP, and WCAP-AS5H.

Lifetime

Lifetime calculator

With this tool you can calculate your maximum expected lifetime. Depending on the product family, a different formula is used for the calculation. This calculator can be found in the aluminum capacitor module on the REDEXPERT platform.

Icon of two parallel capacitors with a clock above, next to the text 'Lifetime Calculator.'

Expected lifetime vs. temperature

In this graph you can find the difference in expected lifetime between our different product families. The curves are based on the different formulas and the endurance of this product. The lifetime table and formula can be found in the information sheet.

Grafik, die das Verhältnis zwischen Temperatur und Lebensdauer von Kondensatoren zeigt.

Webinar

Introduction to the capacitor technologies and how to use them

Webinar

Introduction to the capacitor technologies and how to use them

Capacitors make up two thirds of all electronic components and there is a huge diversity of technologies which can overwhelm young engineers. All capacitors store electrical energy in the electrical field created in a dielectric material and they are used for very diverse applications like voltage stability and filtering. How that works differs between tiny MLCCs and huge electrolytic cells, from pF ratings up to the hundreds of Farads in supercapacitors. In this presentation, we introduce different capacitor solutions taking into account the advantages and disadvantages and with a focus on the final application.

alttext yt_img_for_code_YCVcrKE-6ok.jpg 1745304827

FAQ aluminium capacitors

Datasheet WCAP-CSRF

For most parts you can find the detailed information about packaging in the datasheet: If you cannot find them, please get in contact with Würth Elektronik. E.g. you can use the chat on the website.

Example: Page 3 of WCAP-CSRF component datasheet.


You can find the certifications in the datasheet, page 2.

In the case of X/Y safety capacitors, certification information can be found in PDF format in the online platform REDEXPERT.

These links are shown at the right end of the table, under the column “Certificates”.


We provide the document with all the values on our homepage.

You can also download the document by searching for “FIT” or “MTBF” in our download center.

This document reveals the FIT (Failures in time) and MTBF (Mean time between failures) values that can be calculated for each series based on the electrical stress (voltage applied in the case of capacitors) and the temperature applied according to calculation models of Telcordia SR-332 Issue 3.

Please refer to the table of contents at the beginning of the document to find the values for capacitors.


  1. Würth Elektronik part number
  2. Actual ambient operating temperature which the capacitor is used at (°C)
  3. Operating ripple current flowing through the capacitor (A, RMS)
  4. Frequency of the ripple current (Hz)
  5. Operating voltage which is applied to the capacitor (V(DC))

Table shows the multiplier for ripple current vs frequency

Please find the following example (datasheet, page 2)

For all capacitors of series WCAP-A***, WCAP-P*** and WCAP-H*** there is a maximum ripple current in the datasheet. This ripple current is defined at a specific frequency and temperature and it is given as a RMS (root mean square) value.

Since the ripple current is defined at a certain frequency, it can be converted into the respective value for certain frequencies using factors. These factors can be found in the data sheet.

Let’s assume that the rated ripple current of this part (400V part) is 1 A @ 120 Hz. The max. ripple current @ max. temperature and 10 kHz is then 1.41 A.Furthermore, the ripple current can also be increased if the temperature is below the maximum component temperature. However, this must always be considered in the context of the expected lifetime.

The lifetime calculation in RedExpert can be used for a simple estimate. For detailed considerations, please use one of the many ways of contacting Würth Elektronik to obtain a specific lifetime estimate for your capacitor selection. This value may be increased or decreased if the operating conditions in the application are different from the datasheet.


Extract from the Lifetime calculator in Redexpert

You can find the lifetime calculation on REDEXPERT.

The lifetime calculator may be opened with the sand clock button in the left of the Electrolytic/Polymer/Hybrid . The user must be registered and logged, as this functionality is restricted to registered users.

You can set the conditions in the input box and for Frequency and Temperature you may also move the sliders in the graphs in the right.