Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

12. June 2025
Components

High Mating Cycle Count

Content you may also like

The four new SMT-mountable card connectors

Nano SIM and SD card connectors from Würth Elektronik

Würth Elektronik introduces four new SMT-mountable card connectors and expands its range with solutions for the smallest packages. The four Nano SIM and microSD card connectors feature high-quality workmanship with partially gold-plated contacts and their impressive number of mating cycles mean they have a very long service life.

The new card connectors from Würth Elektronik are each available in two mechanical versions. The WR-CRD Nano SIM Card Connector Push-Push features the familiar spring mechanism, whereby the card is pressed deeper into the slot to release the mechanism. It can be actuated at least 3,000 times. The WR-CRD Nano SIM Card Connector Hinge has a mechanism that withstands no fewer than 5,000 mating cycles.

The microSD cards are available in the WR-CRD MicroSD Card Connector Push-Pull and WR-CRD MicroSD Card Connector Push-Push versions. The Push-Pull version in which the card is held in the connector by friction alone withstands 5,000 mating cycles. Würth Elektronik’s Push-Push version featuring card detection achieves a durability of 10,000 mating cycles.

Compact and robust

Besides telecommunications applications, SIM cards also play a major role in the Internet of Things, as decentralized IoT devices and sensors often use mobile networks to connect to the internet. SD cards frequently serve as exchangeable local storage media for these devices. To address the demands of industrial applications, Würth Elektronik ensures a robust design for its card connectors. The liquid crystal polymer insulating material conforms with the UL94 V-0 flammability class, and the operating temperature range extends from -25 to +85°C – with one version of the WR-CRD MicroSD Card Connector Push-Push even rated for -40 to +85°C.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company information for download

Here you can download the press information and pictures of the company area




Picture material for download

Publications

Reference guides, technical reports and other information material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik blog

Würth Elektronik blog

Learn more about electrical design, new technologies and current innovations in our blog.

You might also be interested in