Press

Welcome to the Press Center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

30. September 2025
Components

Minimal Size, Maximum Flexibility

Content you may also like

One highly compact hardware platform, three variants: the Metis-e, Tarvos-e und Olis-e radio modules

Würth Elektronik presents its Tarvos-e and Olis-e radio modules

Würth Elektronik introduces two new highly compact radio modules. They give developers maximum freedom in designing proprietary wireless solutions that go beyond standard protocols. The hardware of the Tarvos‑e and Olis‑e modules, measuring just 12 Ã— 8 Ã— 2 mm, is identical to that of the Metis‑e radio module and is based on the Texas Instruments SoC CC1310 chipset, operating in the 868 MHz frequency band. Metis-e was introduced at the end of 2024 as a solution specifically for radio transmission of meter readings (wireless M-Bus). Not only their compact design but also the energy-efficient operating modes make the radio modules ideal for use in battery-powered devices. In the Standby and Shutdown power-saving modes, the modules require only 1.6 µA and 200 nA, respectively.

The Tarvos-e module uses Würth Elektronik’s proprietary WE-ProWare radio protocol and is compatible with Tarvos-III and Thebe-II. It allows targeted optimization of wireless communication – either for high data rates up to 400 kbps or for a range up to 2.7 km. It offers maximum flexibility and is ideal for applications for which standard protocols reach their limits. The module delivers an RF output power of 14 dBm and uses a UART interface for communication.

The Olis-e module offers even more design flexibility by allowing you to build your own firmware. Using the TI SIMPLELINK CC13x0 software development kit, developers can implement their application directly on the SoC (System on Chip) – including custom wireless protocols and system logic.

Proprietary radio protocols as a potent alternative to Bluetooth® LE

The radio modules use proprietary protocols and thus offer an especially attractive solution for applications in which both the transmitter and receiver sides are individually developed. Compared to Bluetooth, the module impresses with its greater range – especially indoors – thanks to use of its 868 MHz frequency band instead of 2.4 GHz. This enables more reliable communication, even through walls and other building structure obstacles.

In addition to the standard version in the 868 MHz range, the radio module is also available in a specially adapted variant for the 915 MHz frequency range upon customer request. This option opens up use in markets such as the USA, in which the 915 MHz band can be used license-free.

All three versions (Metis-e, Tarvos-e, Olis-e) include evaluation boards with a USB interface for connecting to a PC, a comprehensive user manual, as well as software tools.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company information for download

Here you can download the press information and pictures of the company area




Picture material for download

Publications

Reference guides, technical reports and other information material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik blog

Würth Elektronik blog

Learn more about electrical design, new technologies and current innovations in our blog.

You might also be interested in