On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik offers WE-CAR-TEC snap ferrites
Waldenburg (Germany), November 22, 2022 – Snap ferrites have helped establish Würth Elektronik's renown as an EMC specialist. Now the manufacturer is launching another line of retrofittable interference suppression solutions with AEC-Q200 qualification, as required for the automotive industry. The WE-CAR-TEC series snap ferrites feature a NiZn core material. WE-CAR-TEC ferrites suppress electromagnetic interference in the frequency range from 1 MHz to 1 GHz.
The internal security locking system prevents unauthorized removal from the cable. Thanks to the “WE-STAR-KEY” key technology, the ferrite is reusable making it ideally suited for test and measuring purposes in the EMC lab. Each packaging unit comes with a “WE-STAR-KEY” to open the snap ferrites. WE-CAR-TEC is available in four different sizes for cable diameters from 3.5 mm to 8.5 mm. The plastic housing is UL94-V0 classified; the operating temperature ranges from -50°C to +105°C.
WE-CAR-TEC is available from stock, free samples are available.
Do You Have Any Questions, Comments or Requests Regarding our Press Work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here You Can Download the Press Information and Pictures of the Company Area
Reference Guides, Technical Reports and Other Information Material
Würth Elektronik blog
Learn more about electrical design, new technologies and current innovations in our blog.