On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik expands its range of coaxial connectors
Würth Elektronik introduces additional coaxial connectors for 50-Ω cables of types 1.13, 1.32, and 1.37 mm. The plugs and receptacles – suitable for use in such equipment as wireless communication devices, GPS systems, and IoT devices – feature gold-plated contacts and have all passed a 48-hour salt spray test. The easy-to-install connectors WR-SMA, WR-SMB, WR-MCX and WR-MMCX are now available from stock without a minimum order quantity.
“WR-SMA Right Angle Bulkhead Jack Cable Connector”: The right-angle receptacle for applications up to 6 GHz features a very space-saving design and reduced cable strain. The new model in the WR-SMA series for crimp assembly is also available in an IP67-rated version.
The “WR-SMB Straight Plug Cable Connector” is similar in size to the SMA version, but is straight and features a snap-lock mechanism. The connector for applications up to 4 GHz is particularly suitable for applications such as test equipment that require repeated mating cycles.
The “WR-MCX Straight and Right Angle Plug Cable Connectors” feature a snap-lock mechanism and are suitable for applications up to 6 GHz. The connectors take up very little space and remain rotatable, which provides added flexibility for the right-angle plug connectors. The connectors have been tested for at least 500 mating cycles. WR-MCX has a connector diameter of 4.5 mm, while the WR-MMCX version has an even smaller diameter of just 3.5 mm. The smaller connector also requires less force both for mating and unmating.
Do you have any questions, comments or requests regarding our press work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here you can download the press information and pictures of the company area










Reference guides, technical reports and other information material
Würth Elektronik blog
Learn more about electrical design, new technologies and current innovations in our blog.