On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
60-V variant of the MagI³C-VDMM MicroModule series
There’s a new generation of MagI³C-VDMM power modules from Würth Elektronik: The ultra-wide input voltage range gives the new MicroModule a robust resistance to voltage transients on the 48 V bus. Its compact LGA-12 package is also conducive to high integration density. The adjustable output voltage ranges from 0.85 to 6 V at a current up to 0.3 A.
The extended input voltage range of the Variable Step Down MicroModule from 3.5 to 60 V now covers bus voltages from 5 to 48 V, opening up applications from Point of Load (PoL) to direct 48 V bus voltage connection. So the MagI³C-VDMM series is ideally suited as a replacement for linear regulators, for example in the power supply of interfaces, sensors, microcontrollers, microprocessors, DSPs and FPGAs. Operational areas include industrial, testing and measurement technology, medical devices and point-of-load DC-DC applications.
Its small footprint and high efficiency (up to 86 percent) supports “cool design”, allowing its use in a temperature range from -40 to +105°C. To save energy, the power module can be set to sleep mode using an additional pin. The very low quiescent current of just 3 µA means the power module is particularly suitable for energy-sensitive applications. The integrated sync feature allows multiple Micromodules to synchronize to an external frequency.
The new MicroModule also meets the requirements of EMC standard EN55032/CISPR32 Class B for radiated and conducted interference with verified filter combinations. The selectively controllable “spread spectrum” feature optimizes EMC behavior.
The new member of the MagI³C-VDMM family is available from stock, even in larger quantities. Free samples can be requested at any time.
Do you have any questions, comments or requests regarding our press work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here you can download the press information and pictures of the company area










Reference guides, technical reports and other information material
Würth Elektronik blog
Learn more about electrical design, new technologies and current innovations in our blog.