On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik updates its online DC-DC Converter Designer
The DC-DC Converter Designer is the most frequently used calculation tool in REDEXPERT. Würth Elektronik has now completely revised and expanded its online service. The heart of the new tool is its proprietary, highly accurate method for calculating inductor losses, based on actual component characterization. It also takes DC-bias effects in inductors and capacitors into account. A new worst-case option for losses and temperature rise provides a valuable tool for robust design that is prepared to deal with all real-world operating conditions.
In practice, the inductance of a core changes significantly as a result of DC bias. Because datasheets often provide only limited information about this behavior, it is easy to select the wrong component.The same applies to ceramic capacitors, whose capacitance decreases significantly under operating voltage. The new DC-DC Converter Designer accurately reflects this reality and provides loss and temperature estimates that more closely reflect the actual behavior on the circuit board.
Automatic topology selection
The tool automatically selects the appropriate circuit topology based on the input parameters: buck (synchronous and asynchronous), boost (synchronous and asynchronous), and SEPIC. A user-defined topology mode is available to experienced users working with specialized or less common circuit topologies. Additional filters for automotive requirements, shielding, and component height simplify component selection for specific applications. A link to the MagI³C Power Module Designer enables users to compare the discrete circuit with an integrated module solution to ensure the optimal solution is selected.
Comparison of enhanced components
The tool’s analytical capabilities have been significantly extended. The system recommends the five most suitable components based on a weighted evaluation of performance and package size. Multiple components can be compared directly: The same graph displays losses as a function of output current (Iout) and switching frequency (Fsw) for all selected components. The graph options have also been significantly expanded: zooming, a crosshair cursor, and exporting as an image or Excel file. Experienced users can manually load any component from across the Würth Elektronik portfolio into the tool without being limited to the automatic recommendation list.
Including capacitor recommendations
The tool now also recommends capacitors and a suitable microchip controller for the specified input parameters. A link to the MagI³C Power Module Designer enables users to compare the discrete circuit with an integrated module solution.
The overview page summarizes all simulation results and generates a complete bill of materials with up to six components. These components can be requested as free samples or added directly to the shopping cart. The DC-DC Converter Designer is available at redexpert.we-online.com.
Do you have any questions, comments or requests regarding our press work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here you can download the press information and pictures of the company area
Reference guides, technical reports and other information material
Würth Elektronik blog
Learn more about electrical design, new technologies and current innovations in our blog.