Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

09. July 2025
Components

High-Frequency Connectors for Antenna Cables

Content you may also like

WR-SMA Right Angle Bulkhead Jack Cable Connector

Würth Elektronik expands its range of coaxial connectors

Würth Elektronik introduces additional coaxial connectors for 50-Ω cables of types 1.13, 1.32, and 1.37 mm. The plugs and receptacles – suitable for use in such equipment as wireless communication devices, GPS systems, and IoT devices – feature gold-plated contacts and have all passed a 48-hour salt spray test. The easy-to-install connectors WR-SMA, WR-SMB, WR-MCX and WR-MMCX are now available from stock without a minimum order quantity.

“WR-SMA Right Angle Bulkhead Jack Cable Connector”: The right-angle receptacle for applications up to 6 GHz features a very space-saving design and reduced cable strain. The new model in the WR-SMA series for crimp assembly is also available in an IP67-rated version.

The “WR-SMB Straight Plug Cable Connector” is similar in size to the SMA version, but is straight and features a snap-lock mechanism. The connector for applications up to 4 GHz is particularly suitable for applications such as test equipment that require repeated mating cycles.

The “WR-MCX Straight and Right Angle Plug Cable Connectors” feature a snap-lock mechanism and are suitable for applications up to 6 GHz. The connectors take up very little space and remain rotatable, which provides added flexibility for the right-angle plug connectors. The connectors have been tested for at least 500 mating cycles. WR-MCX has a connector diameter of 4.5 mm, while the WR-MMCX version has an even smaller diameter of just 3.5 mm. The smaller connector also requires less force both for mating and unmating.

Share:

More news from this business unit

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company information for download

Here you can download the press information and pictures of the company area




Picture material for download

Publications

Reference guides, technical reports and other information material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik blog

Würth Elektronik blog

Learn more about electrical design, new technologies and current innovations in our blog.

You might also be interested in