01. September 2021
Components

Update on IQD’s High Performance Rubidium Oscillator IQRB-2

Content you may also like

Gray cuboid component with blue inscription. In the background you can see a city in the evening light

IQRB-2 rubidium oscillator handbook available now summarising key test data

Waldenburg (Germany), September 1, 2021 – IQD—a Würth Elektronik eiSos Group company— is pleased to announce completion of its extended rubidium portfolio with the comprehensive IQRB-2 rubidium oscillator handbook, summarising tests undertaken: from temperature stability and short-term stability to supply pushing and more.

The IQRB-2 fills the gap between the IQRB-1 and the IQRB-3; the IQRB-1 delivers a superb price performance ratio, whereas the IQRB-3 offers an exceptional phase noise performance paired with a 1 PPS synchronization. The IQRB-2 offers a superb phase noise close to the IQRB-3 performance: a close in phase noise of -108 dBc/Hz @ 1 Hz and a noise floor of -158 dBc/Hz @ 10 kHz and below. Although it does not offer a 1 PPS synchronisation, it is available at a more competitive price vs. the IQRB-3. With a short term stability of 0.0075 ppb @ Tau = 100 s and an aging performance of a maximum of 0.05 ppb per month, the IQRB-2 is still a perfect match for various time and frequency synchronization applications.

For a convenient overview of all IQD’s rubidium products, please refer to our new rubidium flyer available on the Resources page of the IQD website.

For more information on the IQRB-2 or IQD’s rubidium portfolio in general, please visit IQD’s website at www.iqdfrequencyproducts.com. Furthermore, please contact IQD’s sales office if you have any questions or would like to get a copy of the IQRB-2 handbook.

 

Available images

The following images can be downloaded from the Internet in printable quality: https://kk.htcm.de/press-releases/wuerth/

Share:

More news from this business unit