On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik publishes Application Note for interference suppression
Waldenburg (Germany), August 3, 2023 – Würth Elektronik has published a new Application Note: “ANP121 – Filter and surge protection for I2C-Bus”. In this new note, the supplier of electronic and electromechanical components provides valuable support to developers who use the I²C bus (Inter-Integrated Circuit Bus) in cross-circuit-board scenarios. An extension of the interface via connectors or cables can, however, potentially make the I²C bus susceptible to external interference such as electrostatic discharge (ESD), burst, and radiated RF. The purpose of this Application Note is to present a suitable filter and protection circuit that increases the noise immunity of the I²C bus without compromising the signal quality of the data and clock lines.
The latest addition to the collection of application-specific tips on Würth Elektronik’s support sites comprises the sections “Overview I2C bus“, “Overview I2C specifications”, ”Selection of the filter and overvoltage protection components”, “LTspice simulation with 400 kHz clock rate“, and „”Measurement of a real application with 400 kHz clock rate“. The Application Note was created by building simulation models in LTspice and measuring them in a real-life application to verify the results of the simulation.
Test set-up with FeatherWing
To verify the simulation, additional measurements were made on a Würth Elektronik SensorBLE FeatherWing kit. This kit consists of a master board with a microcontroller and two other boards equipped with a WE Bluetooth module and a FeatherWing system with WE sensors (3-axis acceleration, temperature, humidity, pressure). The master board communicates with the other two boards via I²C bus at a maximum data rate of 400 kBit/s. A data cable 20 cm (7.87 inch) long was used to connect the sensor board to the rest of the I²C. A parasitic capacitance of 400 pF with respect to GND was simulated using MLCCs. The simulation and measurement showed that SMT multilayer ferrites in combination with ESD protection diodes have practically no effect on the data signal (SDA) and the clock signal (SCL) of the I²C bus, but rather enhance the noise immunity of the I²C bus.
Do You Have Any Questions, Comments or Requests Regarding our Press Work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here You Can Download the Press Information and Pictures of the Company Area
Reference Guides, Technical Reports and Other Information Material
Würth Elektronik blog
Learn more about electrical design, new technologies and current innovations in our blog.