Filter by values
 in 3 product lines for
Reset all
Filter
Filter by
 show  articles in 3 product lines
 articles in 3 product lines
Reset all
3 Product categories
WE-TVSP Power TVS Diode
WE-TVSP Power TVS Diode
VDC 5 to 440 VIPeak 0.6 to 326.1 A
WE-VS SMT Varistor
WE-VS SMT Varistor
VDC 3.3 to 85 VIPeak 10 to 200 AWmax 0.02 to 1.1 J
WE-VD Disk Varistor
WE-VD Disk Varistor
VDC 18 to 1465 VIPeak 100 to 10000 AWmax 0.7 to 620 J

Surge Protection

Surge Protection

Disk varistors are used in surge protection. It is important that the clamping voltage Vclamp is sufficiently low so that sensitive electronic components in the circuit do not experience voltage spikes. Once the clamping voltage is reached, the voltage hardly increases further; it is "clamped". Steeply rising currents are diverted with low resistance. If the current exceeds Ipeak, it can lead to the destruction of the disk varistor. The maximum operating voltage is significantly lower than the clamping voltage.

The graph depicts the current-voltage behavior of a surge protection diode.

Functionality during normal operation and during overvoltages

In surge protection, a sensitive electronic component (Load) is protected by a parallel discharge path (VDR), which becomes conductive when the breakdown voltage of the protective element (VDR) is reached. In this way, the surge (Transient) does not reach the sensitive load (Load) and is "clamped" to the clamping voltage (Clamping Voltage).

The image shows a circuit that illustrates the use of a voltage-dependent resistor as overvoltage protection.