Measurement & Sensing

Laser

Digital Sensors

Current Sense Transformer

Current sense transformers use the principle of inductive coupling on a transformer to convert the input and output currents and voltages based on turns ratio. The current sense transformer features a primary winding with very few turns, often just one, and a secondary winding with many turns, ranging from tens to thousands. The current passing through the primary winding will induce a current in the secondary winding which can then be converted into a measurable voltage using a burden resistor as the load. Thus, the output voltage is directly proportional to the input current, making the current sense transformer an effective tool for current measurement. Although the current sense transformer is not capable of measuring DC currents, it will measure AC currents with the advantage of offering isolation, common mode noise rejection, accurate measurement and robustness.

Connectors

For measurement and sensing applications, terminal blocks, LED connectors and wire-to-board connectors provide reliable solutions for connecting wires, LEDs, sensors and printed circuit boards. Different pitches, designs and connection technologies enable flexible integration, easy wiring and space-saving designs in electronic devices.

Current Sense Resistors

Current sense resistors are typically resistors placed in series with the circuit through which the current is to be  measured. When current flows through the circuit, a voltage drop occurs across the shunt resistor proportional to the current passing through it. In high-current applications, it can lead to significant power dissipation and heat generation, requiring additional cooling measures or derating of the resistor's power rating. They are typically used in battery management systems, power supplies and converters, motor control and devices.

IR Emitters & Detectors

Infrared emitters and detectors enable non-contact communication and sensing. They are suitable for e.g. remote controls, proximity sensors, and optical data links.

Signal LED

Signal LEDs provide clear visual indication of operating states, warnings, or activity in an electronic system. They are available in various colors and sizes, providing a simple and intuitive status display for users.

Signal LEDs

Pressure Sensors

Short Introduction to Measurement & Sensing

A Sensor is a system that measures a physical dimension and converts it into an electrical signal. Sensors are  analog with infinite resolution, but data to and from  electronic devices is transferred digitally. Analog sensor values must therefore be digitized.

Conversion can be done thorugh a discrete AD converter when using an analog sensor like a Shunt or a Photo-Diode. Alternatively the conversion can be all done within the sensor when using a MEMS system.

The difference between LED and laser: Lasers operate with stimulated emission, while LEDs rely on spontaneous emission. On the left is the light distribution of a VCSEL-type laser. On the right is the typical light distribution of an LED.


Monochromatic ceramic LEDs: Light intensity for different viewing angles. Besides the viewing angle, color also plays an important role.


Light spectrum of different LED types of various colors by wavelengths.


Structure of the infrared LEDs from Würth Elektronik: gold-plated contacts provide excellent connectivity. The LED chips are pre-selected, bonded with gold wires, and tightly encapsulated.


A diagram showing the switching times
Switching times up to 100 MHz

The extremely fast switching time of a few nanoseconds ensures high transmission rates..