Eleazar Falco  - Applications Engineer
Eleazar Falco
Optoelectronics
17. July 2026

Opto-triac operation and design guide

Content you may also like

ANO016 Opto-triac operation and design guide

Optically-isolated TRIACs, also known as opto-triacs or phototriacs, are low-power devices typically used in conjunction with high-power TRIACs to regulate power to loads supplied from the AC-mains, effectively acting as galvanically-isolated, solid-state AC switches. Despite being around for many decades, they are still key components today in several industrial and home-appliance applications, among others.

Starting with a review of thyristor and TRIAC devices, this application note dives into the operation of random-phase (RP) and zero-cross (ZC) opto-triac types, covering their parameters and important design considerations in their target application as a TRIAC driver. In addition, an EMI performance comparison of the two opto-triac types is also included, all accompanied by extensive measurements with the WL-OCTR opto-triac series from Würth Elektronik.

 

Main topics:

  • Background on thyristor and TRIAC devices
  • Operation of Random-Phase (RP) and Zero-Cross (ZC) opto-triacs
  • Opto-triac parameters
  • Opto-triac as an isolated TRIAC driver
  • EMC tests and design considerations

 

Download: ANO016