Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

05. May 2026
Components

Flat Wire and High Efficiency

Content you may also like

The three standard sizes of the WE-SFIA flat-wire inductor

SMT flat-wire inductor for automotive electronics

Würth Elektronik introduces its new WE-SFIA series of flat-wire inductors in 2010, 2013, and 2016 packages. The inductors feature exceptionally low DC resistance and extended operating temperature range from -40°C to +180°C. The WE-SFIA series is available as catalogue components but can also be adapted to meet customer-specific requirements. 

The WE-SFIA inductors are designed for high-efficiency DC/DC converters in the automotive field, such as single- and multiphase converters, as well as buck and boost converters with high saturation currents of up to 150 A. Other filter choke applications include battery management, motor, audio, and infotainment systems.

Flat-wire technology used in the chokes offers a host of advantages: It is mechanically more robust and enables tighter, more even windings as well as improved heat dissipation. Flat-wire windings also offer a larger cross-sectional area, thus reducing electrical resistance. This results in a higher current-carrying capacity, which provides significant advantages in handling transient current peaks. AC losses, such as the skin effect, are also significantly lower in high-frequency applications than in comparable round-wire variants.

Compact and efficient

Thanks to the optimized core material, Würth Elektronik achieves improved magnetic saturation performance with its WE-SFIA inductors compared to other commercial products. The WE-SFIA product series is characterized by its compact design, high temperature resistance, and energy efficiency. This opens up new design possibilities for developers. The flat-wire inductors are available with values from 0.33 µH to 4.7 µH. Further inductance values are available on request.

Share:

More news from this business unit

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company information for download

Here you can download the press information and pictures of the company area




Picture material for download

Publications

Reference guides, technical reports and other information material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik blog

Würth Elektronik blog

Learn more about electrical design, new technologies and current innovations in our blog.

You might also be interested in