Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

05. October 2023
Components

Supplying Terminal Devices via the EMC-compliant Network Connection

Content you may also like

Würth Elektronik presents its reference design for PoE adapter

Waldenburg (Germany), October 5, 2023 – Würth Elektronik is proud to present its RD022 reference design “GB-PoE+ Ethernet USB adapter,” freely available at www.we-online.de/RD022. Devices networked via Ethernet usually depend on a separate power supply, however, if these terminal devices get by with low power consumption, then Power over Ethernet (PoE) is an alternative where data transmission and power supply are achieved via a network cable.

Devices with low power consumption, like IP cameras, VoIP phones, WiFi routers, network switches, LED lighting or access systems, are suitable for power supply through the Ethernet line. Würth Elektronik’s new RD022 reference design, which can provide up to 25W of power, shows how this can work while still maintaining EMC compliance. The ‘GB-PoE+ Ethernet USB adapter’ is based on the reference design of a 1 Gbps Ethernet USB adapter without PoE functionality, as described in detail under RD016 (www.we-online.de/RD016).

The ‘GB-PoE+ Ethernet USB Adapter provides three interfaces: a USB Type-C interface (USB 3.1), an RJ45 1 Gbps Ethernet interface with integrated PoE functionality, and a connection for a DC/DC converter with an adjustable output voltage of 6V to 18V and a maximum output power of 25W. The board makes it easier for customers to get started with PoE technology. The reference design familiarizes users with the technology, signals, interface structure, power-up and PoE detection of a Gigabit PoE interface. It provides the hardware design for Power Sourcing Equipment (PSE) and the Powered Device (PD) and explains the conception and construction of the adapter board: current flow, USB controller and interface, Ethernet interface as well as power supply (PoE). Special importance placed on the EMC-compliant design highlights its significance.

Share:

Content you may also like

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here you can download the press Information and pictures of the company area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik Blog

Würth Elektronik Blog

Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.

You might also be interested in