Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

06. November 2024
Components

For input voltages from 3.5 to 60 volts

Content you may also like

60-V variant of the MagI³C-VDMM family

60-V variant of the MagI³C-VDMM MicroModule series

There’s a new generation of MagI³C-VDMM power modules from Würth Elektronik: The ultra-wide input voltage range gives the new MicroModule a robust resistance to voltage transients on the 48 V bus. Its compact LGA-12 package is also conducive to high integration density. The adjustable output voltage ranges from 0.85 to 6 V at a current up to 0.3 A.

The extended input voltage range of the Variable Step Down MicroModule from 3.5 to 60 V now covers bus voltages from 5 to 48 V, opening up applications from Point of Load (PoL) to direct 48 V bus voltage connection. So the MagI³C-VDMM series is ideally suited as a replacement for linear regulators, for example in the power supply of interfaces, sensors, microcontrollers, microprocessors, DSPs and FPGAs. Operational areas include industrial, testing and measurement technology, medical devices and point-of-load DC-DC applications.

Its small footprint and high efficiency (up to 86 percent) supports “cool design”, allowing its use in a temperature range from -40 to +105°C. To save energy, the power module can be set to sleep mode using an additional pin. The very low quiescent current of just 3 µA means the power module is particularly suitable for energy-sensitive applications. The integrated sync feature allows multiple Micromodules to synchronize to an external frequency.

The new MicroModule also meets the requirements of EMC standard EN55032/CISPR32 Class B for radiated and conducted interference with verified filter combinations. The selectively controllable “spread spectrum” feature optimizes EMC behavior.

The new member of the MagI³C-VDMM family is available from stock, even in larger quantities. Free samples can be requested at any time.

Share:

More news from this business unit

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company information for download

Here you can download the press information and pictures of the company area




Picture material for download

Publications

Reference guides, technical reports and other information material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik blog

Würth Elektronik blog

Learn more about electrical design, new technologies and current innovations in our blog.

You might also be interested in