Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

31. March 2026
Components

Service-Oriented Entry into Cooling Technology

Content you may also like

WE- HIC with continuous fins for applications in which the defined airflow is clearly aligned with the fins.

Würth Elektronik introduces heat sinks for power-electronics and IC components

Würth Elektronik expands its product range and launches a comprehensive heat sink portfolio, divided into three specialized product groups: The WE-HTO heat sinks are designed for THT-TO packages like the TO-220 and TO-247. WE-HIC includes classic finned heat sinks for components with flat surfaces, such as CPUs or DC/DC converters. The WE-HTOI and WE-HICI variants are supplied from the factory pre-coated with thermal interface material. This eliminates the air gap between the component and the heat sink, thus maximizing cooling performance. As a special service, Würth Elektronik provides technical support, detailed heat-sink characteristics, simulation options, as well as customer-specific modifications.

The WE-HTO heat sinks are available in various shapes and with different surface structures to enable tailored cooling performance. These include variants with curved sheet metal and with cooling fins, which dissipate more heat through their increased surface area. In addition, matching M3 screws, nuts, and insulating sleeves for mounting on the WE-HTO and WE-HTOI heat sinks can also be ordered.

Cooling fins for different airflow conditions

WE-HIC is available in two variants: with continuous and interrupted fins. The design with continuous fins is designed for applications in which the airflow is aligned with the fins. The variant with interrupted fins, however, is ideal when airflow in the installation environment cannot be clearly defined. Heat sinks for ICs are available in sizes ranging from 20 × 20 to 40 × 40 mm.

“We’ve been offering thermal interface materials for quite some time now, and in our design-in support for customers we always pay close attention to thermal management as well as EMC. So it’s only logical that we’re now expanding our offering to include heat sinks – after all, preventing overheating contributes to the performance and service life of components,” explains Maria Cuesta-Martin, Product Manager EMC Shielding & Thermal Materials at Würth Elektronik eiSos GmbH & Co. KG.

The heat sinks from Würth Elektronik are now available from stock without a minimum order quantity. Free samples are available on request.

 

Share:

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company information for download

Here you can download the press information and pictures of the company area




Picture material for download

Publications

Reference guides, technical reports and other information material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik blog

Würth Elektronik blog

Learn more about electrical design, new technologies and current innovations in our blog.

You might also be interested in