On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik presents its Setebos-I FeatherWing
Würth Elektronik expands its range of FeatherWings with the Setebos-I radio module. Developers using the practical plug-in boards for fast prototyping benefit from the combined functionality of the manufacturer’s two tried and tested radio modules. Setebos-I combines the features of Thyone-I and Proteus-III, enabling communication via Bluetooth LE 5.1 as well as a proprietary 2.4 GHz radio protocol with mesh networking capability.
The Adafruit Feather form factor allows developers to seamlessly combine Würth Elektronik's growing range of FeatherWings with hundreds of compatible boards from other manufacturers. Setebos-I FeatherWing also has an integrated security element. This IC supports AES128 encryption, ensuring a high level of security and authentication, particularly for IoT applications.
The FeatherWing radio module fully leverages the benefits of the Bluetooth Low Energy 5.1 standard while also offering additional performance features. With a payload of up to 964 bytes, the module delivers four times the throughput of conventional Bluetooth Low Energy modules. In proprietary radio mode, Würth Elektronik shows what is possible in the 2.4 GHz band: a range of up to 750 m and an end-to-end payload throughput of up to 400 kbit/s. A simple setup turns modules into repeaters in a mesh network, as required. The WE-ProWare firmware excels with its powerful, versatile radio protocol and ease of configuration.
Würth Elektronik offers a Wireless Connectivity Software Development Kit (SDK) to complement this product. This also implements all the available commands in pure C code. The radio modules can be effortlessly integrated by porting the corresponding C code to their host processor. This reduces the time needed to develop the software interface for the radio module.
Do you have any questions, comments or requests regarding our press work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here you can download the press information and pictures of the company area










Reference guides, technical reports and other information material
Würth Elektronik blog
Learn more about electrical design, new technologies and current innovations in our blog.