23.10.2025
Webinaraufzeichnung
Englisch

Inrush current of the connector

Inhalte, die Ihnen auch gefallen könnten

All resistors carrying current generate heat, a phenomenon known as the Joule effect. From a thermal perspective, a power connector can be accurately modeled as a simple resistor. The working current of a power connector is typically defined by industry standards, such as UL 1059 in our case, which specifies a maximum temperature rise (∆T) of 30 K (Kelvin is used for temperature difference, while Celsius is for absolute temperature). This implies that at its full working current, the connector's internal temperature will not exceed 30 K above the ambient temperature. The combined temperature rise and ambient temperature are further limited by the maximum operating temperature rating, ensuring connector durability when used with the proper de-rating curve (refer to ANE006 for more details on de-rating). However, certain applications, like the short acceleration phase of an electric scooter, the transition phase of an electric transformer, or capacitance discharge in a lighting ballast, demand a high current for only a brief duration. 

This presentation will address a crucial question for designers: 

  • Do we have to oversize the connector working current to accommodate this inrush current, or is it permissible to temporarily exceed the specified working current for short periods? 
  • Detailed insights into the thermal behavior of connectors under dynamic, high-current pulses. 
  • Guidelines and recommendations for optimizing connector selection in applications with transient overload conditions. 

Presentation: Inrush current of the connector 

Teilen auf:

Noch mehr Videos entdecken?

Auf unserem YouTube-Kanal finden Sie weitere Animationen, TechTalks, Tutorials und Produktvideos sowie alle Webinaraufzeichnungen. Entdecken Sie unser vielfältiges Videoangebot und informieren Sie sich über unsere neuesten Inhalte.

Zwei Menschen vor einem Laptop