22.10.2025
Webinaraufzeichnung
Englisch

ICeGaN™ in LLC Converters: Unlocking performance beyond Silicon for Next-Gen Power Systems

Inhalte, die Ihnen auch gefallen könnten

This paper provides an in-depth analysis of the significant advantages offered by ICeGaN™ technology in high-power LLC converters. These converters are critical for demanding applications such as data servers and on-board chargers (OBCs), where efficiency, power density, and reliability are paramount. The discussion will highlight how ICeGaN™ surpasses traditional silicon (Si), silicon carbide (SiC), and discrete GaN solutions. 

 

Key benefits and technical aspects explored include: 

  • Exceptionally low switching losses and minimal dead times, attributed to ICeGaN™'s inherently low parasitic capacitances and gate charge. 
  • The unique absence of reverse recovery (Qrr), which further contributes to enhanced efficiency. 
  • A distinct feature of not requiring negative gate drive, simplifying gate driver design and operation. 
  • The resulting ability of ICeGaN™ to operate effectively at higher switching frequencies. 
  • The direct impact of these characteristics on achieving increased power density, significant size reduction of converter designs, and improved thermal management. 

Presentation: ICeGaN™ in LLC Converters: Unlocking performance beyond Silicon for Next-Gen Power Systems 

Teilen auf:

Inhalte, die Ihnen auch gefallen könnten