21.02.2022
Webinaraufzeichnung
Englisch

Essentials for the Design of an GB Ethernet Front End

Inhalte, die Ihnen auch gefallen könnten

 

Speaker: Dr. Heinz Zenkner | Duration: appx. 45 min incl. Q&A The webinar describes what is necessary for the development of a GB Ethernet interface, between Phy and Ethernet connector. It goes into detail about the circuit technology, the components and the layout. Points such as matching of the symmetrical signal paths, protection against transient overvoltage, selection of suitable components, design of the ground system, placement of the components on the PCB and layout design are shown, using a practical example. Finally, the topic of EMC is also taken into account.

 

Download presentation now

Teilen auf:

Inhalte, die Ihnen auch gefallen könnten