23.10.2025
Webinar Recording
English

Transformer Safety, update on 61558 standard

Content you may also like

This comprehensive presentation, led by Antwi and Markus, delves into the critical aspects of transformer safety and the methods by which a high level of safety can be achieved in transformer design and application. Understanding and adhering to international safety standards is paramount, especially in power supply units (SMPS) where transformers play a crucial role. The presentation will particularly focus on the IEC 61558 safety standard and its implications. 

 

The session will discuss: 

  • The safety standard IEC 61558 in direct relation to both transformer design principles and their application in Switch-Mode Power Supply (SMPS) units. 
  • The new aspects of the 2021 version of IEC 61558, which is yet to be fully released globally, providing an early insight into future requirements. 
  • A detailed presentation of the various IEC 61558 safety levels relevant to transformer design, specifically addressing: 
  • Overvoltage categories and their impact on insulation requirements. 
  • Precise requirements for creepage and clearance distances to prevent electrical breakdown. 
  • The importance and methodology of the partial discharge test for assessing insulation quality. 
  • The acceptance and harmonization of IEC 61558 with other relevant safety standards, such as IEC 62368. 

Presentation: Transformer Safety, update on 61558 standard

Share on:

Discover even more videos?

On our YouTube channel, you’ll find more animations, TechTalks, tutorials, product videos, and recordings of all our webinars. Explore our diverse range of videos and learn more about our latest content.

Two people in front of a laptop