Press

Welcome to the press center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

17. March 2026
Components

Highly accurate and very versatile

Content you may also like

The WSEN-PDMS differential pressure sensor

Würth Elektronik presents a differential pressure sensor

Würth Elektronik proudly presents their latest product, the WSEN-PDMS, a new highly accurate differential pressure sensor for a multitude of operating scenarios. The sensor operates with an accuracy of ±1 mbar and a resolution of 16 bits, supports a broad voltage range from 3.0 V up to 5.5 V, and is compatible both with digital I²C and SPI communication interfaces as well as an analog interface. Two different casing versions make the sensor particularly versatile: they are available with vertical straight nozzles for connection with pressure adapters and with horizontal barbed nozzles for tube connection. This flexibility makes both system integration as well as prototype development much easier to accomplish.

These features ensure the WSEN-PDMS sensor is compatible with a broad range of microcontrollers and embedded systems. The sensor delivers fully calibrated differential-pressure data as well as optional temperature measurements, and operates reliably in a temperature range from -25°C up to +85°C. Optionally the transmitted measurement results can be complemented by additional CRC bits, thus enabling a reliable and robust communication.

Advanced development

The WSEN-PDMS is based on the robust design of the time-tested WSEN-PDUS sensor, which will remain part of our product portfolio. Just like its predecessor, the new sensor is suited for a broad range of applications – from heating, ventilation, and air-conditioning technology, filter-status monitoring, gas-leak detection, and industrial automation, all the way to medical devices such as inhalation equipment.

Like all the sensor products supplied by Würth Elektronik, the WSEN-PDMS series is also available ex stock without any minimum order quantity. It is also possible to develop versions according to the customer’s own specifications to meet special application requirements. Würth Elektronik offers evaluation boards and an extensive Software Development Kit on GitHub to facilitate a swift development and evaluation process, enabling engineers to put the sensor to use quickly, to test its functionality, and to integrate it into their systems with maximum ease.

Share:

More news from this business unit

Press contacts

Do you have any questions, comments or requests regarding our press work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company information for download

Here you can download the press information and pictures of the company area




Picture material for download

Publications

Reference guides, technical reports and other information material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik blog

Würth Elektronik blog

Learn more about electrical design, new technologies and current innovations in our blog.

You might also be interested in