Speaker: Carlo Lombardi, Microchip Technology | Duration: appx. 45 min incl. Q&A In most of the grid connected applications the auxiliary power supply is normally implemented using the flyback topology. To get the required stabilized voltage(s) a voltage compensator is needed, and in the most of the cases it is implemented on the primary side of the flyback converter. In this webinar a solution based on a primary-side start-up IC (MCP1012) in conjunction with a secondary-side controller is presented highlighting the advanced control techniques that may be implemented using a secondary side controller. Finally a real application for led lighting will be presented.