05.11.2020
Webinaraufzeichnung
Englisch

Derating of connectors - What do you need to consider?

Inhalte, die Ihnen auch gefallen könnten

Derating of connectors - this is the containment of unacceptable heating by the correct use of connectors. Würth Elektronik answers the following questions:


Which connectors are suitable for which application?

How can I optimize a connector and reduce contact resistances?

How many pins can be operated under full load?

What does a derating curve look like and where can I get it?

What influence do the different components of the connector have?

Also take a look at our application manual for optimized connector selection, the "Trilogy of Connectors".

 

Download presentation here

Teilen auf:

Inhalte, die Ihnen auch gefallen könnten