14.03.2024
Webinar Recording
English

Simplify Filter Calculation and Selection with REDEXPERT EMI Filter Designer

Content you may also like

REDEXPERT Filter Designer is suited for input filters for DC-DC converters, AC-DC converters, but also output filters. The tool is very useful to design a differential mode input filter or specific noise filter without going into complex filter calculation. Instead of using trial-and-error for determining the components needed to create the filter, the REDEXPERT EMI Filter Designer does all the calculations based on a few input parameters. It uses the non-ideal component models, which includes the parasitics, to determine the performance of the filter and takes into account system impedances. Using the correct input parameters, as described, the tool can reduce the process of making a design EMC compliant in time and cost.

 

Presentation Simplify Filter Calculation and Selection with REDEXPERT EMI Filter Designer

Share on:

Content you may also like