On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Würth Elektronik presents its optical sensors for object recognition
Würth Elektronik launches a new program for optical sensors (product code: WL-OSEN) with the first two components. These compact modules contain both emitters and detectors for infrared light at 940 nm wavelength. A special feature: The Würth Elektronik sensors filter out visible light up to 800 nm, rather than just up to 700 nm as is the case for many other sensors of this type available on the market. So they are less susceptible to errors occurring under artificial lighting.
The sensor in the 4-SMD gullwing standard housing measures 2.7 × 3.4 × 1.5 mm without contacts. It is designed for close range, typically at a distance of 1 mm and serves as a simple touch switch, for example under a glass plate. The second compact SMD sensor, with its lower beam angle and measuring 2.0 × 1.6 × 0.75 mm, can detect at a greater distance up to 10 mm, making it more robust against crosstalk than a simple touch switch, e.g., when used under glass. Both sensors offer an analog output and low energy consumption. Possible applications include optical encoders, switches and interlocks, as well as object detection or touch applications.
The Würth Elektronik infrared sensors are now available from stock without a minimum order quantity. Developers can receive free samples.
Do you have any questions, comments or requests regarding our press work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here you can download the press information and pictures of the company area
Reference guides, technical reports and other information material
Würth Elektronik blog
Learn more about electrical design, new technologies and current innovations in our blog.