On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Wi-Fi module for IoT security
Würth Elektronik introduces its new Cordelia-I Wi-Fi module, specifically designed for secure IoT and ‘edge computing’ applications. This versatile module is ideal for applications in Industry 4.0, Smart City / Smart Home, eMobility, smart agricultural, and medical devices, to name a few. It meets the requirements of RED (Radio Equipment Directive) including the Cybersecurity Regulation 2022/30 in accordance with EN 18031-1, which will become mandatory for all devices with radio technology in the EU as of August 2025. The Cordelia-I module was developed in collaboration with British cybersecurity company Crypto Quantique – to ensure the highest security standards. With a compact size of just 19 × 27.5 × 4 mm, it is designed to operate over a temperature range of -40 °C to +85 °C, and consumes less than 10 μA in standby mode.
The new Wi-Fi module from Würth Elektronik independently manages secure cloud connections, thus reducing the workload on the host MCU. MQTT over TLS is used as the primary protocol for connecting to the cloud. The module features a secure Root of Trust (a fundamental security concept in information technology) that is unique and tamper-proof. All cryptographic keys are securely generated and stored within the module.
Cordelia-I supports cloud connectivity via Crypto Quantique's QuarkLink platform, ensuring secure and scalable zero-touch provisioning as well as cloud onboarding of the end device in the field. This SaaS platform (Software as a Service) allows implementation of the first security layer for an IoT device. The necessary steps include: secure provisioning of devices, onboarding with a cloud service provider or an in-house server-based application, and managing the devices throughout their lifecycle.
The Cordelia-I module complies with the IEEE 802.11 b/g/n Wi-Fi standard and operates in the 2.4 GHz band. In Transparent Mode, it provides a secure UART-to-Cloud bridge. The transmission power goes up to +18 dBm (peak), while the receiver sensitivity is -92 dBm.
Würth Elektronik offers an evaluation kit, SDK and PC tools for evaluation of this product as an additional service. This simplifies the development of hardware and software for IoT applications using Cordelia-I.
Do You Have Any Questions, Comments or Requests Regarding our Press Work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here You Can Download the Press Information and Pictures of the Company Area
Reference Guides, Technical Reports and Other Information Material
Würth Elektronik blog
Learn more about electrical design, new technologies and current innovations in our blog.