13. May 2026
Components, Intelligent Systems

Solutions for Modern Power Electronics

Content you may also like

The Würth Elektronik booth team looks forward to welcoming numerous visitors.

Würth Elektronik at PCIM Europe 2026

Würth Elektronik is exhibiting at PCIM Europe in Nuremberg from June 9 to 11, 2026, at Booth 306 in Hall 6. With its portfolio, ranging from high-current contacts and thermal management to components for line filter applications, the company will present itself as a partner for developers. This spirit of partnership extends to the booth, which will be operated jointly by Würth Elektronik eiSos (Electronic and Electromechanical Components) and Würth Elektronik ICS (Intelligent Power and Control Systems). Reference designs developed together with various IC partners will also be presented. As in previous years, Würth Elektronik is also contributing presentations and a seminar to the PCIM conference program.

Würth Elektronik eiSos will be exhibiting products such as high-frequency inductors with high efficiency and innovative core materials to complement its proven ferrite-based series. Also on display will be high-current inductors with flat wire and components for modern line filter applications. A key topic will be ferrites for protecting PCBs from high inrush currents and for DC/DC conversion. Also on display is a brand new line of heat sinks for power electronics and IC components.

Seminar with an EMC expert

Würth Elektronik eiSos is contributing to the PCIM conference program with its specialists, including a seminar by renowned EMC expert Dr. Heinz Zenkner (Designing Robust Industrial Interfaces: Advanced Strategies for Transient Protection, Arvena Park Hotel, June 7, 2026, 2:00–5:30 p.m.) and a presentation by Alexander Gerfer, CTO of the Würth Elektronik eiSos Group (AI and Electronics – Trends, Challenges, and Urgent Opportunities, Stage Tokyo, Level 3, June 10, 2026, 11:30–11:50 a.m.).

More details on the rest of presentation program are available on
https://www.we-online.com/enpcim2026.

Reliable high-current connections for modern power electronics

Würth Elektronik ICS specializes in high-current contacts for PCBs in power electronics, particularly lead-free Powerelements. The focus is on the LF PowerBasket, a pluggable high-current contact rated up to 150 A that features high positional tolerance and low mating forces, which is often used for reversible board-to-board connections. Another highlight is PowerBusbars, application-specific busbars for locally increasing current-carrying capacity and improving heat dissipation. The trade show innovation PowerBusbar PF consists of vertically press-fit busbars that act like cooling fins and dissipate heat particularly efficiently. These vertical busbars can be used as a current path or current bridge.

Share: