Blog

Marketing Team - Editorial team
Marketing Team
Printed Circuit Boards, Sustainability, Research & Development
19. May 2026

Cellutronik: when bacteria become the starting point for printed circuit boards

Content you may also like

Image shows a cellulose mass held in the hands of an R&D colleague wearing blue gloves

Sustainability in electronics is no longer a future topic—it has become a concrete development task. With the research project Cellutronik, Würth Elektronik Circuit Board Technology, together with the University of Stuttgart and the Hahn-Schickard Society, is taking it a step further: toward bio-based substrate materials and digitized manufacturing processes for next-generation printed circuit boards.

The project is funded by the German Federal Ministry of Research, Technology and Space (BMFTR) and officially started in November 2025.

Bacterial cellulose as a new material base

At the core of Cellutronik is an unusual approach: bacterial cellulose as a substrate material for printed circuit boards. This material is produced in the laboratory using microorganisms and then processed into stable, board-like structures.

The idea behind it is clear: to replace petroleum-based materials in electronics in the long term and thereby significantly reduce environmental impact across the entire product lifecycle.

From lab material to industrial application

Turning a material concept into a real technological option requires more than basic research.

  • The University of Stuttgart is developing suitable processes for producing cellulose fibers.
  • Hahn-Schickard is working on additive manufacturing methods and digital printing technologies.
  • Würth Elektronik Circuit Board Technology contributes its expertise in industrial PCB manufacturing.

The focus is not only on the “if,” but above all on the “how”: How can a new material be integrated into existing production processes?

Digital manufacturing directly on the substrate

A key component of the project is the use of modern printing technologies. Conductive structures are applied directly to the cellulose surfaces using inkjet printing. Copper and silver inks form precise conductive traces exactly where they are needed.

The result:

  • reduced material consumption
  • less waste
  • shorter process times
  • new design freedom in PCB development

An additional advantage: both substrates and conductive traces are solderable and therefore fundamentally compatible with existing assembly processes.

Industry and research working hand in hand

Cellutronik follows a clear principle: research should not end in the lab.

Instead, industrial applicability is at the center from the very beginning. This is exactly where the value of the collaboration emerges—new technologies are developed in a way that makes them transferable to real manufacturing environments in the long term.

This approach reflects the development philosophy of Würth Elektronik Circuit Board Technology: innovation driven by real customer requirements and industrial processes.

Outlook: demonstrator for multilayer PCBs

At the end of the project, a demonstrator is planned that will showcase the production of multilayer printed circuit boards based on cellulose and digital printing processes.

It is intended to demonstrate that:

  • sustainable PCB substrates are technically feasible
  • digital manufacturing opens up new design possibilities
  • ecological benefits and industrial requirements can be combined

In the long term, Cellutronik pursues an ambitious goal: enabling electronic solutions that generate significantly less environmental impact at the end of their lifecycle.

Conclusion

Cellutronik demonstrates how strongly material innovation and manufacturing technology can influence each other. What still sounds like research today could become an important building block for more sustainable electronics of tomorrow.

Content you may also like