21. May 2021
Intelligent Systems

Valuable Practical Knowledge for Developers in Power Electronics

Content you may also like

Würth Elektronik ICS is holding a free online seminar on

Würth Elektronik ICS High Current Contacts Webinar

On June 2nd 2021, Würth Elektronik ICS will be hosting a free online seminar on the topic of "high current contacts in power electronics". The speaker Günter Behlau, project engineer in the components department at Würth Elektronik ICS, will present various high-current contacts, processing guidelines for them and recommended design rules for their use. You can register under Webinar "High current contacts in power electronics"

The field of power electronics is currently experiencing strong growth and is being increasingly used in more and more applications. E-mobility being the most prominent example. Power electronics applications include electrical drive technology or converters requiring the safe handling of high currents. Cable connections, busbar contacts, board-to-board connections or component connections all require correspondingly robust contacting solutions. In addition, contacts and PCB must be optimally matched to each other.

In the webinar, Günter Behlau will explain various aspects that are important in high-current contacting. Special attention will be paid to mounting methods to the PCB, including soldering and press-fit technology. The fixing of the contacts to the application, for example by means of plugging or screws is also relevant. In order to guarantee the reliability of the overall system, certain design rules must be observed with the design of the overall system influencing both the current-carrying capacity and mechanical stability.

Tips from the Inventor of Powerelements

With Powerelements, Würth Elektronik ICS has performed important pioneering work in the field of high-current contacts for PCBs - and is now doing so again with a lead-free product line "LF Powerelements". Using these, developers can reduce the documentation effort (REACH, SCIP) and make designs free of the uncertainty surrounding the future of the RoHS Exemption Directive 6c. As such, there is no risk of a possible re-design at a later point in time. The lead-free high-current contacts, available as standard or customised solutions, can be used in not only in the automotive sector, but also in many fields including medical technology and household appliances. By working closely with their customers, the experts at Würth Elektronik ICS have experience with many practical applications - and thus with the practical strengths and weaknesses of various designs. "In the webinar, we provide an insight into our technologies and pragmatically describe the design guidelines for high-current contacts in conjunction with the PCB. We provide information on the reliability of the systems and show various interesting practical solutions. I am already looking forward to the feedback from the webinar participants," says Würth Elektronik ICS expert Günter Behlau.

Registration under Webinar "High current contacts in power electronics"

Share:

Content you may also like