Thermal simulation for MagI³C Power Modules using RedExpert

This webinar gives an introduction into the online design tool REDEXPERT® for MagI³C Modules. Focus of the webinar is on the self-developed thermal tool for REDEXPERT®. With this tool, the power dissipation and surface temperature of the MagI³C Power Module can be determined and heat distribution on the entire PCB can be uniquely displayed on a heat map. Finally, an example of a thermally optimized module selection with REDEXPERT® is given using a concrete application, to show the added value of thermal simulation during the design-in phase.

<< Back to all webinar recordings

Also take a look at our application manual, the "Abc of Power Modules".

Also read our application note "DNS004: MagI³C Power Modules".

Discover our innovation campaign "All inclusive" for MagI³C Power Modules.

Würth Elektronik Webinar: Thermal simulation for MagI³C Power Modules using REDEXPERT