Search results

  • 100%

    ICCS Software Tools

    For programming of our ICCS CAN products we offer a software tool ICCS SDK Plus . Programming In the development phase, we offer support in creating programs. Also you can create programs by yourself using the software development kit ICCS SDK Plus . We can provide you a Try & Buy Kit for three month free of charge. In the series phase, we supply the ICCS small controllers and ICCS CAN bus controllers pre-programmed with the required functions. We are constantly working on the optimisation and functionality  [...]

  • 99%

    Würth Elektronik ICS presents REDline Power Boxes

    [...]  are used. The benefits of the platform concept at a glance The platform concept behind the REDline Power Boxes enables the broadest range of applications to be realized and requirements to be met. The housing is standardized – which means that tooling costs are eliminated. The individual layout and customized configuration of the circuit boards ensures the highest possible degree of functionality. The cover of the housing can be fitted and removed without the need for extra tools. High IP protection [...]

  • 99%

    Find the right coils for wireless power transfer

    Würth Elektronik eiSos presents its Mix and Match selection tool Würth Elektronik eiSos is the manufacturer with the world’s broadest product spectrum of wireless power charging coils. Now the company provides developers with a tool to simplify selection of the right transmitter and receiver coils. Mix and Match , like the world's most precise AC loss calculator for power inductors, is another offering from the REDEXPERT Toolbox. Also like the other tools in REDEXPERT, Mix and Match shows online  [...]

  • 99%

    Software Downloads

    You can download the appropriate software files for all our Wireless Connectivity products. Here you will find the software files: PC-Tools PC-Tools, which allow to configure and evaluate WE wireless connectivity modules via PC and USB connection. Please note that the modules Calypso, Proteus-I, Proteus-II and Triton are not configurable with the ACC-Tool. ACC AT commander tool Smart commander tool WENSS - Würth Elektronik Navigation Satellite Software Software Development Kit Software development  [...]

  • 99%

    ICCS SDK Plus

    For programming of ICCS CAN controllers we have developed the ICCS SDK Plus . With this tool, you can easily program functions similar to how you create schematics. Since the CAN controllers have a flash memory, they can be reprogrammed several times. ICCS SDK Plus consists of a visual programming module and the USB-to-CAN adapter from Peak, which allows you to transmit a programmed function to the CAN controller. With the visual programming module you can create your own program without any C code.  [...]

  • 98%

    ICCS Try & Buy Kits

    Creating programs for ICCS CAN Controllers itself is quite easy: just use the Try & Buy option for the software development tool ICCS SDK Plus . Thanks to included hardware and corresponding interfaces between soft- and hardware you can use the Try & Buy kit: To create the programs for ICCS products easily on your own For development purposes For pilot series For service work For tests You can test the Try & Buy kit for three month free of charge, without any obligations. Afterwards, it can be returned  [...]

  • 98%

    Find the right coils for wireless power transfer

    Würth Elektronik eiSos presents its Mix and Match selection tool Würth Elektronik eiSos is the manufacturer with the world’s broadest product spectrum of wireless power charging coils. Now the company provides developers with a tool to simplify selection of the right transmitter and receiver coils. Mix and Match , like the world's most precise AC loss calculator for power inductors, is another offering from the REDEXPERT Toolbox. Also like the other tools in REDEXPERT, Mix and Match shows online  [...]

  • 97%

    Controllers

    [...]  solution, or can be used to enhance existing CAN networks. ICCS CAN Relays ICCS CAN I/O ICCS CAN Controllers ICCS CAN Gateways Function Specific Modules are used to fulfill defined functions: Voltage Reference Solid State Relay ICCS Software Tools With software tools ICCS SDK Plus the ICCS CAN controllers can be programmed. In addition, we provide supporting tools such as our Try & Buy Kits to help you to create programs. ICCS SDK Plus ICCS Try & Buy Kits

  • 97%

    6 Way Symbol Cluster CAN

    [...]  symbols and colors can be easily implemented. Applications Add-on features indicators Standard symbol cluster based on CAN communication Vehicle functions visualization Technical Data CAN Bus Inputs/ Outputs Features und configuration tool Hardware map Pin Assignment Dimensions Project procedure Order information Technical Data General Information Connector Micro Fit 6 Ways MPC3 Dimensions 24 x 97 x 20 mm Weight 21 g Operating temperature -30 °C to 80 °C Storage temperature -40 °C to 85 °C Ingress [...]

  • 97%

    Intelligent Power and Control Systems from Würth Elektronik

    [...]  up an individual consultation with us today! Power management Customer-specific power distributors REDline Power Boxes REDline Central Electrical Unit Control ICCS Small Controllers ICCS CAN bus Controllers Function Specific Modules ICCS Software Tools HMI WEcabin Displays LED Symbol Clusters High Current Terminals Powerelements Powerelement Online Shop SKEDD Connecting Solutions Wire-to-Board Board-to-Board Component-to-Board

  • 97%

    Design FAQs: Flex-rigid

    [...]  radii are possible in general but have to be designed and qualified for every application individually. We would like to assist you. Please note that the specifications in the design rules "FR4 Semiflex" regarding bending direction and bending tool must be regarded. How much is the maximum ampacity in the flexible or semiflexible area with same load on all conductors? This question cannot be answered in this way. For the current carrying capacity the IPC-2152 "Design guideline for the determination [...]

  • 97%

    FAQs: Flex-rigid

    [...]  radii are possible in general but have to be designed and qualified for every application individually. We would like to assist you. Please note that the specifications in the design rules "FR4 Semiflex" regarding bending direction and bending tool must be regarded. How much is the maximum ampacity in the flexible or semiflexible area with same load on all conductors? This question cannot be answered in this way. For the current carrying capacity the IPC-2152 "Design guideline for the determination [...]

  • 97%

    Webinars Thermal management

    Here you find the presentations of past Thermal management webinars for download or for repeated viewing. Thermal management - a decisive aspect in the development of LED applications Options for cooling components such as LEDs and high-power transistors using a circuit board Thermal simulation helps in choosing the right thermal management concept Insulated Metal Substrate (IMS): a portrait Cooling Tool;[...]

  • 97%

    Webinars Thermal management

    Here you find the presentations of past Thermal management webinars for download or for repeated viewing. Thermal management - a decisive aspect in the development of LED applications Options for cooling components such as LEDs and high-power transistors using a circuit board Thermal simulation helps in choosing the right thermal management concept Insulated Metal Substrate (IMS): a portrait Cooling Tool;[...]

  • 97%

    REDline Power Boxes

    [...]  of the printed circuit board and thus the functionalities. With the platform concept of the REDline Power Boxes various applications can be implemented and requirements can be fulfilled. The access to serviceable components can be done without tools, as well as the lid mounting. There is also the possibility to integrate a label into the lid. Additionally, every box includes integrated compression limiters. The high IP protection classes guarantee a high degree of security. Custom-specific projects [...]

  • 97%

    SKW - Connector

    Features Currents up to 20 A at 85°C Connector with 2, 3 or 4 chambers Repeatedly pluggable without tools Large air and creepage path for high voltages Design with houd for contact protection and secure locking Secure prepositioning through pilot pin on casing Sample Reques Data sheet Electrical parameters Current carrying capacity 20 A at 85 °C Voltage max 500 V Contact resistance < 0.5 mΩ Mechanical parameters Mating cycles 5 Grid 5.0 mm (offset) Wire cross-section 1.0 mm² to 2.5 mm² Insertion  [...]

  • 97%

    History

    [...]  initial staff of 11. 2013 In December 2013, the SKEDD direct plug-in technology is presented to the public. With this innovative technology, connectors and components can be connected and disconnected from the circuit board directly and without any tools. 2014 In 2014, the new technology and production center of Würth Elektronik ICS GmbH & Co. KG is inaugurated. All five previous locations in the area of Hohenlohe are now working in a modern building in the industrial park Waldzimmern in Niedernhall. [...]

  • 97%

    Layout & Design

    It is necessary to start thinking about suitable measures to dissipate heat already in the design and development phase. In general, it is much more expensive to implement modifications and adaptations at a later point in time. A thermal simulation of the printed circuit board can help you choosing the best printed circuit board construction and the optimal layout in advance. The following tools will help you choosing the right thermal management concept: Design Guide Webinars FAQ [...]

  • 97%

    SKEDD Direct Plug-In Technology

    SKEDD technology is a connection technology in which connectors and components can be connected and disconnected directly to a printed circuit board without tools. Thus, SKEDD offers a simple and reliable alternative to other PCB connection technologies. Visit the SKEDD website to learn all about SKEDD technology, the SKEDD contact and qualification. Are you interested in our SKEDD technology connecting solutions ? Then contact us! SKEDD Flyer Business Models Customer specific connector systems We  [...]

  • 97%

    Würth Elektronik ICS expands ICCS portfolio

    [...]  allow a pass-through design of the wiring harness. The module is also equipped with poly fuses (2×3 A and 1×5 A) for protected supply of external devices. The two modules are programmed with ICCS SDK Plus , Würth Elektronik ICS’ development tool. ICCS SDK Plus enables graphical programming using function blocks. Alternatively, the program can be created using the C programming language. Würth Elektronik ICS supports its customers in the creation of programs. Customers can order an ICCS SDK [...]

  • 97%

    Würth Elektronik ICS awards licence for SKEDD technology to Diehl Metal Applications

    [...]  directly to a circuit board – without an adapter – can also be connected and disconnected over the course of many cycles. Diehl Metal Applications develops and manufactures customized solutions across the entire value-added chain: prematerial, tool manufacturing, stamping technology, S+D press-fit zones, plating technology, and metal-plastic compaind systems. By using SKEDD, the company will expand its portfolio of connection technologies between contact systems and circuit boards. "For DMA, [...]

  • 97%

    Design advantages 

    [...]  holes are generally used together on a circuit board Each technology offers advantages in layout. However, laser-drilled microvias is an additional process that generates costs. Direct comparison of the variable production costs (tool costs, processing costs, energy, etc.) between microvias (Ø 125 µm hole / 300 µm pad) and mechanically-drilled vias (Ø 300 µm hole / 550 µm pad) shows that the substitution of approx. 180 mechanically-drilled vias per dm² with microvias represents the breakeven [...]

  • 96%

    Publications

    [...]  with integrated laser scanner unit Application Note Flex-Rigid 2,415KB [icon] Flex-rigid circuit board in audio systems: High frequencies without crosstalk Application Note Flex-Rigid 2,843KB [icon] Reliable flexrigid-solution for robust industrial tools Application Note Flex-Rigid 2,597KB [icon] Flex-rigid pcb for very limited space applications Application Note Flex-Rigid 2,724KB [icon] The TWINflex® construction principle: Convincing Flexible Possiblilities! Application Note Flex-Rigid 1,982KB [...]

  • 96%

    Download Center

    [...]  with integrated laser scanner unit Application Note Flex-Rigid 2,415KB [icon] Flex-rigid circuit board in audio systems: High frequencies without crosstalk Application Note Flex-Rigid 2,843KB [icon] Reliable flexrigid-solution for robust industrial tools Application Note Flex-Rigid 2,597KB [icon] Flex-rigid pcb for very limited space applications Application Note Flex-Rigid 2,724KB [icon] The TWINflex® construction principle: Convincing Flexible Possiblilities! Application Note Flex-Rigid 1,982KB [...]

  • 96%

    Download Center

    [...]  with integrated laser scanner unit Application Note Flex-Rigid 2,415KB [icon] Flex-rigid circuit board in audio systems: High frequencies without crosstalk Application Note Flex-Rigid 2,843KB [icon] Reliable flexrigid-solution for robust industrial tools Application Note Flex-Rigid 2,597KB [icon] Flex-rigid pcb for very limited space applications Application Note Flex-Rigid 2,724KB [icon] The TWINflex® construction principle: Convincing Flexible Possiblilities! Application Note Flex-Rigid 1,982KB [...]

  • 96%

    Webinars Flex-rigid

    [...]  Flex-rigid: design rules as success factor The benefits of flex-rigid Base materials and their characteristics Flex-rigid in combination with USB3 Flex-rigid: design mistakes and their effects Current flex-rigid standards Flex-rigid in the EDA tool Semiflex: An award-winning miniaturization success Flex-rigid - on course right from the start Flex-rigid designs thorough checkup Flex-rigid designs thorough checkup (part II) Collaboration with Altium - joint webinar on flex-rigid technology, part 1 [...]

  • 96%

    Webinars Flex-rigid

    [...]  Flex-rigid: design rules as success factor The benefits of flex-rigid Base materials and their characteristics Flex-rigid in combination with USB3 Flex-rigid: design mistakes and their effects Current flex-rigid standards Flex-rigid in the EDA tool Semiflex: An award-winning miniaturization success Flex-rigid - on course right from the start Flex-rigid designs thorough checkup Flex-rigid designs thorough checkup (part II) Collaboration with Altium - joint webinar on flex-rigid technology, part 1 [...]

  • 96%

    Würth Elektronik starts APPLAUSE

    [...]  and testing experts launched a new project, “Advanced packaging for photonics, optics and electronics for low cost manufacturing in Europe,” simply called APPLAUSE. The project fosters the European semiconductor value chain by building new tools, methods and processes for high volume manufacturing. The 34M€ total budget for the three-year project is co-funded by Horizon 2020 and national funding agencies and industries, as a part of the Electronics Components and Systems for European Leadership [...]

  • 96%

    Flex-rigid circuit boards: Standard for the third dimension

    [...]  circuit boards FR4 semiflex More in the design guide! Areas of application Typical fields of application for this type of technology include industry, automotive, aeronautical engineering and medical technology. It can be used for sensors, tools and vision systems, especially with the USB 3.0 standards with UL certification. Our expertise – your profit! The circuit board is no longer thought of as simply something to hold other elements. In fact, it is part of the system and offers a diverse range [...]

  • 96%

    Thermal management

    [...]  heat. There are a number of different possible ways to design systems for the heat dissipation of components. They always have to be individually executed and they have to be adapted to the different requirements of the assembly. The following tools show you how you can incorporate this technology into your system. Design Guide Webinars Contact Product Manager

  • 96%

    Printed Polymer

    [...]  development process from the earliest possible stage. This helps us to find the right solution for the customer’s specific requirements and keep an eye on the entire system. Learn more about the printed polymer application options. The following tools show you how to include this technology into your system. Design Guide Design Tip Webinars Contact the product manager

  • 96%

    Wirelaid 3D Design Rules

    [...]  + 200 μm K Solder mask clearance in bending area 1.0 mm R Thickness of residual material Thickness of wire + copper + solder mask + 150 μm Wires need to be arranged at right angles to the bending area The usage of an applicable bending (forming) tool is recommended Bending radius ≥ 0.1 mm Care has to be taken so that the bent parts are secured in the installed application to avoid further movement

  • 96%

    FAQs: Basic Design Guide

    [...]  pad size? Usually the final drill diameter is specified to be 0.35mm smaller than the pad size. The PCB manufacturer usually drills 0.10mm greater than the specified final diameter and uses a theoretical residual ring of min. 125µm, based on the tool diameter. Thus, a drill diameter of 0.15 mm is appropriate for a 0.55mm via pad. The respective standard values are listed in the Basic Design Guide . Plated through hole vias: What are the copper clearances that should be adhered to on inner ground [...]

  • 96%

    Würth Elektronik ICS presents REDline Power Boxes

    [...]  are used. The benefits of the platform concept at a glance The platform concept behind the REDline Power Boxes enables the broadest range of applications to be realized and requirements to be met. The housing is standardized – which means that tooling costs are eliminated. The individual layout and customized configuration of the circuit boards ensures the highest possible degree of functionality. The cover of the housing can be fitted and removed without the need for extra tools. High IP protection [...]

  • 95%

    Wurth Electronics Midcom at the APEC 2016

    Components, tools, and presentations by partners Represented by its US subsidiary Wurth Electronics Midcom, Würth Elektronik eiSos will be exhibiting at the APEC (Applied Power Electronics Conference) in Long Beach, California (20–24 March 2016). The component supplier will be occupying stand #1933 of the Long Beach Convention & Entertainment Center to present its extensive range of products: from capacitors, via SMD ferrites, all the way to the world’s smallest power inductors made of magnetic  [...]

  • 95%

    Toolbox

    With the help of the following tools & tutorials we facilitate the component search and selection for you: Design Software Search Tools Infographics Libraries Tutorials Design Software Discover Würth Elektronik's online platform for simple component selection and performance simulation. Try REDEXPERT and calculate your losses in real-time Analog IC Selector : The manufacturer independent parametric IC search with focus on SMPS Monolithic Power System DC/DC-Designer Texas Instruments WEBENCH® Designer  [...]

  • 95%

    Using the Gap Calculator

    [...]  gap by two for the thickness of the gap spacer. Going even further, users can manually modify the core area and the magnetic path lengh for experimental puposes. Just by choosing another pakcage, the program will reset to default values. About the Tool The Wurth Electronics Midcom Gap Calculator is an easy way to quickly calculate the gap length once the desired AL value and the package are known. Along with the information on the gap length, this tool also provides a quick access to other useful [...]

  • 95%

  • 95%

    No suitable assembler?

    Find the suitable assembler with our assembler pool Behind the assembly pool are cable assemblers tested by Würth Elektronik: experts for the processing of our connectors. Always close to you throughout the country. No matter the size: All our cable assemblers are equipped with tools that guarantee a high-quality processing of our connectors. We from Würth Elektronik establish the connection to our assembling partners, suitable to your request. Manual Cable Assembly for Initial and release samples  [...]

  • 95%

  • 95%

    Components and Services for Electronics of the Future

    [...]  system solutions, reference designs and the REDEXPERT simulation software, with which engineers in electronic companies can quickly and easily find the suitable component for their application. The component selection assistant from the REDEXPERT tool is not only based on simulations, but also on extensive measurement series in typical applications and therefore delivers more accurate results. Other themed islands are devoted to EMC and inductive automotive products from Würth Elektronik iBE, the [...]

  • 95%

    Electronic Components for Power Tools

    [...]  for PCB Assembly - USB Type C 3 Capacitors - Fuseholders 4 Quartz Crystals & Oscillators REDCUBE Terminals 5 Sensors - DC Power Jacks 6 LEDs - Detector Switches 7 Tact Switches - Bluetooth - Wireless Power - Proprietary - Resistors - DC Power Tool Würth Elektronik Components No. Components No. Components 1 Surge Protection 10 Switches 2 Film Capacitors - Single Coil Power Inductors 3 Common Mode Chokes - Ferrites for Cable Assembly 4 Aluminium Electrolytic Capacitors - Varistors 5 Resistors - REDCUBE [...]

  • 95%

    Products & Services

    [...]  have come to the right place: New Products Innovations Applications We want to offer you the best service & support. Here you will find all our offers that will make your work easier: Service: Everything you need for delivery, ordering and support Toolbox: More applications, tools and helpful materials at a glance Quality: Our standards plus ISO, REACh & RoHS certificates for download Application Notes: Practical Application & Design Notes on various topics Component Libraries: Download 3D data [...]

  • 94%

    Service - more than you expect!

    [...]  Added Values Discover the online platform REDEXPERT for simple component selection and performance simulation The free iOS Würth Elektronik App for component search and selection helps you to find the corresponding product for your aplication Toolbox: Search & Software Tools for engineers and developers You can attend on our design seminars and webinars free of charge EMC Test lab search engine Explore our Toolbox with Search & Software Tools! In addition, we offer you special added values for [...]

  • 94%

    Silicon Labs' EFM32 Giant Gecko Starter Kit (EFM32GG-STK3700)

    [...]  a SEGGER J-Link debugger Energy Debugging with an integrated Advanced Energy Monitoring (AEM) with Voltage Monitoring Please follow these steps to start your evaluation Download Simplicity Studio Install Simplicity Studio – it contains all the tools, drivers, software examples and documentation needed, like energyAware Commander - a tool for updating the kit's firmware, programming the MCU on STK or on your prototype energyAware Profiler – energy debugging and supply voltage monitoring tool ;[...]

  • 94%

    Wurth Electronics’ REDEXPERT Tool Launches Flyback Transformer Selector

    Wurth Electronics is pleased to announce the launch of their Flyback Transformer Selector in the newest release of their REDEXPERT tool. The integration of the Transformer Selector into REDEXPERT is a complete makeover of the original Smart Transformer Selector. This free tool is available in seven languages and requires no login. More options are included in the REDEXPERT tool, including performance simulation, filter settings for over 20 electrical and mechanical parameters, direct access to product  [...]

  • 94%

  • 94%

    AnDAPT: AnD7220EB Adaptable PMIC Buck

    The AnD7220EB is a ready to use Evaluation Boardsto evaluate the Dual-Buck AnD7220. Simply apply PVIN, then measure default settings of 0.7V on the VOUT terminals. To change VOUT, adjust the resistor divider ratio according to: R2 = Vfb * R1 / ( VOUT-Vfb) kΩ, or use the WebAdapter tool and select your desired VOUT. The tool reports will provide the resistor required location and value. To access the WebAdapter tool, please use the following link . Optionally, the Bucks may be modified as needed  [...]

  • 94%

    A connection for life: Crimping part 2

    Illustration 1: kabelforum.de A connection for life: Crimping part 2 The first part of our blog introduced ‘crimping’ as a connection technique. In this part 2 we will delve deeper to help those who order parts and tools from Würth Elektronik achieve the best crimping results. The crimping process: Step 1: The die is open. A connector is placed on the anvil. The wire is inserted by hand or by machine. Step 2: The descending crimper presses the wire into the crimp barrel and catches the crimp  [...]

  • 94%

  • 94%

    A Connection for Life: Crimping

    [...]  strands. Next, the insulation is stripped off. Tip: If possible, use V-knives, not flat knives Our next blog about quality control will highlight what could go wrong during the crimping process. What is very clear already is that you need the right tools to achieve the right crimp connection. Naturally the required tools are offered by Würth Elektronik: • Manual Crimping Tool: We offer manual crimping tools with die and positioning aid, where rolling of the crimp edge is done by the crimp die. [...]

  • 94%

    Wurth Electronics Midcom at the APEC 2016

    Components, tools, and presentations by partners Represented by its US subsidiary Wurth Electronics Midcom, Würth Elektronik eiSos will be exhibiting at the APEC (Applied Power Electronics Conference) in Long Beach, California (20–24 March 2016). The component supplier will be occupying stand #1933 of the Long Beach Convention & Entertainment Center to present its extensive range of products: from capacitors, via SMD ferrites, all the way to the world’s smallest power inductors made of magnetic  [...]

  • 94%

  • 94%

    WE Backup Your Application – A real life Supercapacitor backup solution

    [...]  power rail application. The available output power is 30 W (12 V @ 2.5 A). We also talk about the classification of Supercapacitors, the model parameters and performance and of course the charge-, discharge and frequency behavior. We have different tools to support your design-in process. For example the Support Note SN009, the Application Note ANP077 and currently we working on a Supercapacitor bank calculation tool. WE support you in your Design. For the power stage, we used the software for and [...]

  • 94%

    Select the Right Transformer

    What's important in your magnetics? Creating the perfect transformer is hard, especially when there are so many factors to consider. Wurth Electronics Midcom has put together a few useful tools to help you in your design process. The first took we have is an interactive infographic that will help lead you on the right path to picking your ideal transformer. You can view that here . The second tool we have is a series of blog posts that will inform you about the considerations one must take when designing  [...]

  • 94%

    Gap Calculator Desk Tool released by Wurth Electronics Midcom

    Wurth Electronics Midcom Inc announced the release of a new online tool: the Gap Calculator. The Gap Calculator tool provides a quick calculation of the gap length of a transformer’s core once the desired AL value and the package are known. To use the Gap Calculator, a user must first choose the desired package from the drop-list. Then, insert the AL value in the correct field. From here, the calculated gap can be extracted from the “Actual” field. For a feasible gap, the resulted value is  [...]

  • 94%

    Privacy & Data Protection Policy

    [...]  as cookies are saved for the analysis of your usage habits, these are treated separately in this privacy policy. Details on cookies, as well as an overview of the cookies used can be viewed on the page "Cookie guidelines" . c. Use of web analytics tools (1) Google Analytics This Website uses Google Analytics, a web analysis service of Google Inc., Mountain View, CA, USA. (“Google”). Google Analytics uses various methods to analyse the use of a website, such as “cookies” (see Section 3b. [...]

  • 94%

    Würth Elektronik eiSos publishes the RED EXPERT online design tool: the world's most precise AC loss calculation

    With RED EXPERT, Würth Elektronik eiSos has published a new online tool with which developers can simulate the power inductors from Würth Elektronik. With just a few clicks, the power inductors are selected and the complete AC losses calculated. The special feature: RED EXPERT enables the world's most precise loss calculation, because it is not based on the known Steinmetz models with sinusoidal excitation, but rather is derived and validated from measurements of the power inductors in a switching  [...]

  • 94%

    Selecting the Right Wireless Power Coils

    Würth Elektronik eiSos expands Mix and Match selection tool Würth Elektronik eiSos is the provider with the world’s broadest product spectrum of wireless power charging coils. The company places a tool at developers’ disposal which facilitates selection of the appropriate transmitter and receiver coils. Mix and Match is a free-of-charge offering from Würth Elektronik eiSos. As with REDEXPERT – the world’s most precise AC loss calculator for power chokes – the product specifications accessible  [...]

  • 94%

  • 94%

    Gleanergy Demonstration Kit at Energy Harvesting & Storage USA in November 2016

    [...]  both high power and low power, and their applications. The event brings together the complete value chain, from technology developers to integrators to end-users, providing insight on market trends, latest products and emerging technology toolkits. At this year’s EHS USA held from November 16-17 in Santa Clara, CA, visitors can experience a deeper understanding of Gleanergy. Get registered if you haven’t already and visit our booth where we will be featuring this new board! For further information [...]

  • 94%

    Eager Anticipation Ahead of Berlin – Europe Plays Host to the Formula E Race Series

    [...]  the battery is integrated in the electric racer. The parent company has also become inspired by Formula E: in a joint project with Adolf Würth KG and Würth Elektronik eiSos GmbH & Co. KG, the assembly professional Würth manufactured mobile tool racks especially for ABT Schaeffler Audi Sport and supplies the appropriate tools. Download press release and pictures here: www.htcm.de/kk/wuerth Overview TV broadcasting times and streams via social media channels TV Thursday, 8th June 2017 6:00 pm german [...]

  • 94%

    Expanded range of webinars

    [...]  Participation is free of charge and the registration does not entail any further obligations. Dates, topics and speakers 28.04.2020 Fundamentals of GNSS positioning and receiver technology 28.04.2020 Selection of a Common Mode Choke via our online tools (language: French) 29.04.2020 Selection of a Common Mode Choke for data lines via our online tools (language: French) 30.04.2020 Selection of a Power Inductor via our online tools (language French) 30.04.2020 EMC Shielding 101: Designer's Approach [...]

  • 94%

    Informational and educational activities about passive components

    Würth Elektronik eiSos supports EPCI Würth Elektronik eiSos is pleased to announce its cooperation with and support for the European Passive Components Institute s.r.o. (EPCI). The cooperation includes the development of easy-to-use web-based tools for designers of passive component hardware, educational tools for schools, and promotion of the passive components industry to everyone interested in this field. Würth Elektronik eiSos has become a gold sponsor of EPCI and co-sponsor of the upcoming  [...]

  • 94%

    Request for Crossreference

    Please fill out the form and you will receive information of a suitable component of Würth Elektronik  [...]

  • 94%

    BMBF project KoSiF started - companies and researchers working together on flexible and autonomous sensor systems

    [...]  Fine and Microtechnology (IZFM) for 14 years in the field of MID technology for constructing plastic-based multifunctional 3D packages with a high level of miniaturisation and complex 3D requirements. HSG-IMAT has particular experience in precision tool-making and the ultra-precision processing of optical components, micro injection moulding, transfer moulding and simulation, the metallisation of MID with chemical and PVD processes, laser-based microstructure technologies, 3D assembly and assembly [...]

  • 94%

    Providing 3-D, Eagle, and LTspice files

    [...]  There are several different programs for simulating in the market. One of the most popular and easiest ones is Linear Technology’s Spice program, or LTspice, which is free of charge. Wurth Electronics Midcom has been supporting this software tool from the early stages. So you can see that all of our products are included in the LTspice libraries, especially components like inductors, ferrites, and transformers. All of our products that can be simulated are included in this library and are available [...]

  • 94%

    Component Selection Based on Measured Data

    Würth Elektronik eiSos online design platform REDEXPERT extended Würth Elektronik eiSos has extended its free online design tool REDEXPERT. The simulation software, which has become known as the world's most precise option for AC loss calculation in switch mode power supplies, now supports calculations for a whole range of other components. LEDs for horticultural applications, wireless modules, photodiodes and foil capacitors are among the product groups now included in the simulation tool. The  [...]