Snap Ferrites from Würth Elektronik
In-house product development of the STAR series at
the highest level
Würth Elektronik eiSos invests in innovative and new products - right from the start.
During the last years, especially in the field of snap ferrites, many innovations could be developed, patented and brought onto the market.
Customers all over the world appreciate the high quality and reliability of our products, which are backed by standardized processes, international quality centers and engineering specialists.
Find out more about the in-house developments in the area of the snap ferrite STAR series here:
Patent Number: | EP1689078B1 | EP0981856B1 | EP1039632B1 |
---|---|---|---|
Period of time: | 1999 - 2019 | 1999 - 2019 | 2000 - 2020 |
Description: | Lock inside the housing and only the opening of the lock with key is possible. | In the corners of the housing halves there are pins which are inclined to the corners. When the ferrites are inserted, these ferrites are held with these pins. | Cable fixing which holds the flat cable in the open housing. |
STAR-RING | ✓ | ||
STAR-BUENO | ✓ | ||
STAR-FLAT | ✓ | ✓ | |
STAR-TEC | ✓ | ✓ | |
STAR-FIX | ✓ | ||
STAR-FIX LFS | ✓ | ||
STAR-GAP | ✓ |
Patent Number: | EP1632042B1 | EP2024979B1 | EP2630648B1 |
---|---|---|---|
Period of time: | 2004 - 2024 expected | 2007 - 2027 expected | 2011 - 2031 expected |
Description: | Has a spacer element which creates an air gap. | Deformable cable prefixation for different cross sections and stabilities. | Breakthrough to see the correct lock, right after closing. |
STAR-GAP | |||
STAR-BUENO | ✓ | ||
STAR-FLAT | |||
STAR-TEC | ✓ | ||
STAR-FIX | ✓ | ||
STAR-FIX LFS | ✓ | ||
STAR-GAP | ✓ | ✓ |