FAQs
- I want to collect energy from more than one source at the same time. How can I achieve it?
You can achieve one or more sources by using diodes instead of one jumper (JP1 to JP4) as indicated in the board schematic. - Do I need to buy a separate debugger/programmer to use the EFM32 GG Starter Kit?
The EFM32 Development Kits and Starter Kits include an integrated J-Link device for debugging and programming. The kits are connected directly to a computer through USB, and can handle debugging and programming of the EFM32. You can also debug and program an EFM32 device on your own circuit board. - Where can I find code examples for the EFM32 microcontrollers?
Simplicity Studio includes source code for several code examples. Find out how to install Simplicity Studio by following the steps in this article. Under the 'Examples' category in Simplicity Studio you will find several examples, sorted by kit. The 'Application Notes' category contains all the application notes for the EFM32 microcontrollers, which also include source code examples.
More FAQs can be found here.