Press

Welcome to the Press Center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

13. February 2025
Components

Extra slim 2.4 GHz radio module

Content you may also like

Thyone-e is an especially compact and cost-effective proprietary radio module

Würth Elektronik introduces its Thyone-e

The Thyone I radio module from Würth Elektronik now has a little sibling: Thyone-e, which takes up 30 percent less space and represents a cost-effective alternative for applications in which the long-range mode is not required. Like the other radio modules in the series, Thyone-e can be used to set up mesh networks, radio-based maintenance interfaces, and sensor networks in IoT and M2M applications. The WE-ProWare firmware from Würth Elektronik, which has been proven over many years, makes the chipsets extremely versatile as proprietary radio modules.

Thyone-e has an integrated PCB antenna and an RF pad for connecting an external antenna. It achieves a line-of-sight range of up to 350 meters. There is a choice between a 1 Mbps and a 2 Mbps radio profile. The module, measuring just 7 × 9 × 2 mm, can be used for unicast, multicast, or broadcast data transmission and offers AES128 encryption. Thyone-e achieves up to +4 dBm output power and is highly energy-efficient: The current consumption in standby mode is less than 0.4 µA.

Würth Elektronik offers evaluation boards, a wireless connectivity software development kit, as well as the WE-UART terminal for this product. This easy-to-use PC software allows complete control of the Würth Elektronik radio modules via an intuitive GUI. Together with the evaluation boards, the tool enables rapid prototyping and testing of various functions.

Thyone-e is available from stock without a minimum order quantity.

Share:

Content you may also like

Press contacts

Do You Have Any Questions, Comments or Requests Regarding our Press Work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here You Can Download the Press Information and Pictures of the Company Area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik blog

Würth Elektronik blog

Learn more about electrical design, new technologies and current innovations in our blog.

You Might Also be Interested in