Press

Welcome to the Press Center of Würth Elektronik

On this page you will find information and images for your journalistic reporting.

If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.

03. June 2025
Components

Two Radio Protocols – One Module

Content you may also like

The Skoll-I wireless module combines Bluetooth® Classic und Bluetooth® LE in a compact module.

Würth Elektronik presents its Skoll-I Bluetooth® module

Manufacturer of electronic and electromechanical components, introduces Skoll-I, a compact wireless module that combines both Bluetooth® Classic and Bluetooth® LE (Low Energy) version 5.4 in a single solution. Measuring just 16.6 × 12 × 1.7 mm, the module is already certified for conformity in all major target markets, accelerating the launch of new applications.

Würth Elektronik’s new Bluetooth® Classic / Bluetooth® LE module with integrated antenna is suitable for use in medical devices, industrial automation and control systems, in security technology and IoT clients such as cost-efficient predictive maintenance. These applications typically require energy-efficient operation.

Small and versatile

Combining Bluetooth® Classic and Bluetooth® LE in a compact module offers a unique opportunity for developing devices that need to connect to both legacy and modern devices. Skoll-I also offers an easy way to replace the Puck-I Bluetooth® module, which can no longer be qualified for new developments due to the withdrawal of the Bluetooth 2.0 specification.

Skoll-I complies with Bluetooth® Core Specification Version 5.4 and supports BR, EDR 2/3 Mbps, Bluetooth® LE, and LE 1/2 Mbps. The module is certified to CE, FCC, IC, TELEC, and ETA-WPC standards.

Compelling all-in-one package

The WE Bluetooth® LE Terminal App provides a quick and easy way of testing as well as the basis for developing new, custom apps. Additional services include the Wireless Connectivity software development kit (SDK), the WE UART terminal, and an evaluation board that can be easily connected to a PC to provide access to all module pins for testing.

Immediately available

Skoll-I is now available from stock with no minimum order quantity and is suitable for SMT assembly thanks to its tape-and-reel packaging. Free samples can be requested at any time.

Share:

Content you may also like

Press contacts

Do You Have Any Questions, Comments or Requests Regarding our Press Work?

Electronic & Electromechanical Components

Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com

Printed Circuit Boards                                                                    

Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com

Intelligent Power and Control Systems                       

Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com

Company Information for Download

Here You Can Download the Press Information and Pictures of the Company Area




Picture Material for Download

Publications

Reference Guides, Technical Reports and Other Information Material

  • Reference Guides

    We have recorded our knowledge and know-how in various reference guides.

  • Application Notes

    Practical application & design notes from the electronics expert including help with schematics, EMC, reference notes and technical support.

Würth Elektronik blog

Würth Elektronik blog

Learn more about electrical design, new technologies and current innovations in our blog.

You Might Also be Interested in