On this page you will find information and images for your journalistic reporting.
If you have any questions, please feel free to contact us personally at any time. Here you find our Press contacts.
Stay Connected
Waldenburg (Germany), January 19, 2023 – Würth Elektronik now presents its “Electromechanical Components 2023” catalog to download. The catalog contains 65 pages with innovations from the areas of connection and assembly technology as well as switches and buttons. The manufacturer dedicates a chapter to the REDCUBE high-power contacts. Thanks to press-fit technology, they are particularly robust and vibration-resistant. All products in the catalog can be ordered from stock without a minimum order quantity. Developers can receive free samples on request.
The new catalog clearly shows the various options for connecting PCBs with one another or with cables. A highlight in the 2023 catalog is the M12 circular connectors with screw locking and IP67 or IP68 protection for data lines in industrial automation equipment. The coaxial connectors also include an interesting new arrival: various N-type coaxial connectors to the MIL-STD-348 standard for particularly rugged applications. Among the switches, a new toggle switch family catches the eye—with a current carrying capacity of 1 A, rated voltage of 30 V and ESD compliance with IEC 61000-4-2.
REDFIT CRIMP is a particularly stable yet reversible connection for up to 16 A and 400 V. This PCB connector uses Würth Elektronik patented SKEDD technology. A positioning pin allows non-rotating connection to the PCB by hand and without a mating connector.
The printed version of the catalog can also be ordered at:
https://www.we-online.com/en/products/components/service/information-components
Components
Components
Würth Elektronik has connectors independently tested for fire resistance
Continue Reading
Components
Components
Starke Partnerschaft in der Region
Continue Reading
Components
Components
Würth Elektronik expands its series of signal transformers for large energy storage devices and UPS
Continue Reading
Do You Have Any Questions, Comments or Requests Regarding Our Press Work?
Würth Elektronik EMV & Inductive Solutions
Sarah Hurst
Phone: +49 7942 945-5186
E-mail: sarah.hurst@we-online.com
Würth Elektronik Circuit Board Technology
Melanie Wöhrle
Phone: +49 7940 946-5932
E-mail: melanie.woehrle@we-online.com
Würth Elektronik Intelligent Power & Control Systems
Sandra Herter
Phone: +49 7940 9810-1503
E-mail: sandra.herter@we-online.com
Here You Can Download the Press Information and Pictures of the Company Area
Reference Guides, Technical Reports and Other Information Material
Learn More About Electrical Design, New Technologies and Current Innovations in Our Blog.