ICCS SDK Plus

For programming of ICCS CAN controllers we have developed the ICCS SDK Plus. With this tool, you can easily program functions similar to how you create schematics. Since the CAN controllers have a flash memory, they can be reprogrammed several times.

ICCS SDK Plus consists of a visual programming module and the USB-to-CAN adapter from Peak, which allows you to transmit a programmed function to the CAN controller. With the visual programming module you can create your own program without any C code.

You reduce your development and implementation time significantly. The visual programming module is based on Eagle software of Autodesk.

Important Note!

You need the Eagle software for graphical programming. You can download the new version Eagle 8 according to your needs and requirements at: http://www.autodesk.com/products/eagle/overview. There you can choose between a free version, which you can use for testing purpose, or an Eagle Standard or Premium version with a subscription.

The creation of the programs in the programming language C is possible without restrictions.