STAR-Series

Patents of the Würth Elektronik STAR-Series

Patentnummer: EP1689078B1 EP0981856B1 EP1039632B1
Anmeldejahr: 1999 1999 2000
Beschreibung Lock inside the housing and only the opening of the lock with key is possible. In the corners of the housing halves there are pins which are inclined to the corners. When the ferrites are inserted, these ferrites are held with these pins. Cable fixing which holds the flat cable in the open housing.
STAR-RING    
STAR-BUENO    
STAR-FLAT  
STAR-TEC  
STAR-FIX    
STAR-FIX LFS    
STAR-GAP    
Patentnummer: EP1632042B1 EP2024979B1 US9066415B2
Anmeldejahr: 2004 2007 2010
Beschreibung Has a spacer element which creates an air gap. Deformable cable prefixation for different cross sections and stabilities. Breakthrough to see the correct lock, right after closing.
STAR-GAP      
STAR-BUENO    
STAR-FLAT      
STAR-TEC    
STAR-FIX    
STAR-FIX LFS    
STAR-GAP