Header
Header

How a photovoltaic system works

These days, modern living also includes environmentally friendly and efficient energy supply. Utilising the sun's energy is especially important in this regard. Photovoltaic systems "capture" the light and convert it into electrical energy.
This "capturing" is based on a physical process in which the sunlight shining on a module is converted into electrical energy.
If sunlight shines on a semiconductor (e.g. silicon or CIS), charge carrier pairs are generated. Positive and negative particles are created. These charge carriers are separated by an internal electrical field. This creates areas with a surplus of electrons and areas with a shortage of electrons. If you connect a consumer (such as a light bulb) between the plus and minus poles, a direct current (DC) flows.

When solar cells are interconnected electrically, we call this a solar module.
All the electrically connected modules together produce a solar generator. An inverter converts the direct current generated by the solar generator into alternating current (AC) and feeds this into the public grid – and there you have a "simple" photovoltaic system.
The quantity of energy fed to the grid is recorded by a feed meter.

How a photovoltaic system works

The sun's energy fluctuates throughout the day and also according to the season, but regional factors, such as geographical location, shadows from trees, etc., also affect the quantity of energy that is generated.


What are the main components of a photovoltaic system?

  • Solar generator (electrically connected modules)
  • Frame (mechanical mount for the solar generator)
  • Inverter (converts solar direct current into alternating current)
  • Feed Meter (records the energy fed to the public grid)

Other advantages of a photovoltaic system:

  • GeneCIS photovoltaic modules are noise and odour free
  • GeneCIS photovoltaic modules can be elegantly integrated into the roof, regardless whether it is a new or existing building
  • GeneCIS photovoltaic modules contribute to appealingly designed and modern supply security.
  • GeneCIS photovoltaic modules provide reliable solar power for the next 20 to 30 years

Have we awakened your interest? We will be happy to advise you.

TRADE FAIRS 

Visit us at these trade fairs. We look forward to meeting you.

link_bullet more

PORTFOLIO

Here you can obtain information about our portfolio.

link_bullet more

9 46 00-0

CONTACT

Do you have any questions? We will be more than happy to answer them.
Phone +49 (0)791 9 46 00-0 or e-mail wuerth-solar@we-online.de